How to change microcontroller in exsisting project in S32 DS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to change microcontroller in exsisting project in S32 DS

1,251 Views
baseerahmadpiracha
Contributor III

Is there any way to change the microcontroller in S32 DS IDE. 

For example if I have a project for S32K144 microcontroller can I convert it or make compatible with S32K146 microcontroller.

 

#S32K #NXP

Tags (4)
0 Kudos
Reply
3 Replies

1,242 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@baseerahmadpiracha

I see what you mean, but it's probably not okay,
If it is a different package of the same chip, it can be replaced directly, only need to do some simple modifications

0 Kudos
Reply

1,238 Views
baseerahmadpiracha
Contributor III

Can you please share the modifications I can make to run S32K144 project on S32K146 micrcontroller.

0 Kudos
Reply

1,235 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@baseerahmadpiracha

Senlent_0-1677144114175.png

 

0 Kudos
Reply