How is it possible for ADC to gets trigeered in STOP1 Mode ??

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How is it possible for ADC to gets trigeered in STOP1 Mode ??

跳至解决方案
1,317 次查看
KARTHKSARODE
Contributor III

Hi Team 

I was exploring the Demo projects of S32K144 SDKs , In adc_low_power_s32k144 Demo project 

For power saving purpose , they are going into STOP1 mode & whenever ADC operation is finished , they are coming back to RUN mode again

But my Question is , how can ADC module be active in STOP1 mode , as ADC module is in OFF mode in STOP1 mode (PFA)

Screenshot (22).pngScreenshot (23).png

Please me in clarifying these points 

 

Regards

Karthik SV

Best Regards
KARTHIK SV
标记 (2)
0 项奖励
回复
1 解答
1,304 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@KAPTHKSAPODE

           This Demo project use LPIT to pre-trigger adc-conversion,the LPIT module can work in low-power mode,so I think that this does not conflict with the content described in the data sheet.

BR!

     Jim,

---------------------------------------------------------------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
---------------------------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,305 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@KAPTHKSAPODE

           This Demo project use LPIT to pre-trigger adc-conversion,the LPIT module can work in low-power mode,so I think that this does not conflict with the content described in the data sheet.

BR!

     Jim,

---------------------------------------------------------------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
---------------------------------------------------------------------------------------------------------------------------------------

0 项奖励
回复