How do I set a pin of S32K344 to open drain output mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How do I set a pin of S32K344 to open drain output mode

Jump to solution
1,266 Views
SCoder41
Contributor III

How do I set a pin of S32K344 to open drain output mode.We have designed the hardware to be in an open drain output triggered mode, with a 5V pull-up,Our hardware schematic is shown in the following figure

7.png

0 Kudos
Reply
1 Solution
1,229 Views
PavelL
NXP Employee
NXP Employee

Hello @SCoder41 ,

important is RTD version. If you look to the link in the first reply, there is function 

void Siul2_Port_Ip_SetPinDirection(Siul2_Port_Ip_PortType * const base, uint16 pin, Siul2_Port_Ip_PortDirectionType direction);

which can help you.

Best regards,

Pavel

View solution in original post

0 Kudos
Reply
6 Replies
1,253 Views
PavelL
NXP Employee
NXP Employee

Hello @SCoder41 ,

there's no "true" open drain support on S32K344 (GPIO open drain? - NXP Community). But your application doesn't look like time critical (many MHz), so you can manage open drain mode easily by switching GPIO between "HighZ" mode and "ouput low" mode.

Best regards,

Pavel

0 Kudos
Reply
1,236 Views
SCoder41
Contributor III
S32DS3.5
0 Kudos
Reply
1,240 Views
SCoder41
Contributor III
How to set GPIO to "HighZ" mode
0 Kudos
Reply
1,230 Views
PavelL
NXP Employee
NXP Employee

Hello @SCoder41 ,

important is RTD version. If you look to the link in the first reply, there is function 

void Siul2_Port_Ip_SetPinDirection(Siul2_Port_Ip_PortType * const base, uint16 pin, Siul2_Port_Ip_PortDirectionType direction);

which can help you.

Best regards,

Pavel

0 Kudos
Reply
1,161 Views
SCoder41
Contributor III
Which address should the first parameter of the function 'Siu l2 Port Ip_SetPinDirection' point to?
0 Kudos
Reply
1,154 Views
PavelL
NXP Employee
NXP Employee

Hello @SCoder41 ,

here's example for PTG29:

#include "Siul2_Port_Ip.h"

Siul2_Port_Ip_SetPinDirection(PORTG_H_HALF, 29-16, SIUL2_PORT_HI_Z);

16 shall be subtracted for the upper half port numbers.

Best regards,

Pavel

0 Kudos
Reply