How can i modify ADC for multiple channel interrupt?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How can i modify ADC for multiple channel interrupt?

1,978件の閲覧回数
Sukumar21
Contributor III

I am using s32k146 EV board, there is an sample code given RTM 4.0.3 adc_hwtrigger_s32k146.

I tried this code for ADC. IT works perfectly. But using same code how can i read ADC for multiple channels.

I want to modify the same code for 8 channel ADC, with ADC channel been used are SE06/07/08/09 and SE12/13/14/15 for ADC0.

 

タグ(4)
0 件の賞賛
返信
3 返答(返信)

1,947件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@Sukumar21

We have a similar discussion on the link below, you can refer to the demo in the link attachment.

https://community.nxp.com/t5/S32K/How-to-use-ADC-internal-supply-monitoring/m-p/1346544 

1,929件の閲覧回数
Sukumar21
Contributor III

This is an swTrigger example, this is good. but i am looking utilise interrupt either adc or pdb. so is there sample code with adc interrupt or using PDB

0 件の賞賛
返信

1,916件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信