How can I CAN RX Interrupt example ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How can I CAN RX Interrupt example ?

4,056件の閲覧回数
jaewoosong
Contributor III

I proceed project by using S32K144.

I find CAN RX Interrupt example in this community. But that example is not maked based on processor expert.

So it is difficult to merge my project with example. I hope to find CAN RX Interrupt example by using processor expert.

(Not polling example)

Thank you.

タグ(1)
4 返答(返信)

3,476件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

The SDK demo example in S32DS is using interrupt for RX and TX operation. You can refer to it. Examples are called CAN_MASTER_Example and CAN_SLAVE_Example.

BR, Petr

3,476件の閲覧回数
jaewoosong
Contributor III

Thank you for help

0 件の賞賛
返信

3,476件の閲覧回数
huaping
Contributor III

Dear Jaewoo:

         Have you run CAN RX interrupt example  sucessfully? If yes, is it possible to share the example?

         Thanks!

3,476件の閲覧回数
kimjunghyun
Contributor III

Hi. Petr Stancik.

Do you mean this code is interrupt?

* from CAN_SLAVE_Example

2.jpg

Kim

0 件の賞賛
返信