HomePlug Green PHY communication via power line

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HomePlug Green PHY communication via power line

716 Views
JasonTseng
Contributor I

Hello,

By using nxp s32k and connect to QCA7000, it can transmitting and receiving data over the power line.
Now my setup is s32k as a master in the SPI protocol, with the QCA7000 acting as a slave. I am able to read/write qca register from LPC side. Next step is Powerline Communication.


Question: If start to transmit data to power line, what kind of signal can be measured?

Thanks

Tags (1)
0 Kudos
Reply
1 Reply

681 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

this seems to be question for QCA7000 functionality, so rather ask its support line directly.

BR, Petr

0 Kudos
Reply