HomePlug Green PHY communication via power line

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HomePlug Green PHY communication via power line

660件の閲覧回数
JasonTseng
Contributor I

Hello,

By using nxp s32k and connect to QCA7000, it can transmitting and receiving data over the power line.
Now my setup is s32k as a master in the SPI protocol, with the QCA7000 acting as a slave. I am able to read/write qca register from LPC side. Next step is Powerline Communication.


Question: If start to transmit data to power line, what kind of signal can be measured?

Thanks

タグ(1)
0 件の賞賛
返信
1 返信

625件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

this seems to be question for QCA7000 functionality, so rather ask its support line directly.

BR, Petr

0 件の賞賛
返信