HVBMS s32k358 project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HVBMS s32k358 project

Jump to solution
1,600 Views
BillWen
Contributor III

Hi :

Currently, I try to develop BMS system based on s32k358 platform. I already refer the "HvBms800_774_772_TPL_Bring_Up" source code to develop.

Back to original code and EVB from NXP, I use this project and run on NXP RD-K358BMU board, I found that GeneralError would return error after system run about half to one hour. The error always related to SL layer part such as "ERROR_CMU_READ_MEASUREMENTS_SME3_ERROR".

I wonder know that is there a project or bring up source code without SL part? Because I can't figure out the problem. Really need NXP's help, thanks a lot.

 

Thanks

BR, BillWen

1 Solution
1,517 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi BillWen,

Here is the feedback from HVBMS team:

Inside the Bms SL demo part there is a counter that limits the usage to a number of calls, to protect against production usage of demo SW.  This feature is inside our SW since the first release in 2021.

So this is the intended behavior of our SW to avoid this, the customer should buy the premium.

If they do not then, they will have to handle the TD extraction by their own.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

2 Replies
1,518 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi BillWen,

Here is the feedback from HVBMS team:

Inside the Bms SL demo part there is a counter that limits the usage to a number of calls, to protect against production usage of demo SW.  This feature is inside our SW since the first release in 2021.

So this is the intended behavior of our SW to avoid this, the customer should buy the premium.

If they do not then, they will have to handle the TD extraction by their own.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

1,597 Views
BillWen
Contributor III

Hi:

Updated attach files which is NXP example project "HvBms800_774_772_TPL_Bring_Up"

thanks

BR, BillWen

0 Kudos
Reply