HVBMS EB Tresos Project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HVBMS EB Tresos Project

944 Views
Shivanand
Contributor II

Hello @nxp

I'm trying to setup EB Tresos for HVBMS project of s32k358. In the following steps they have mentioned to add compiler path and Tresos tool path. In Compiler path it is mentioned to add GHS compiler which is commercial , can I use GNU compiler. If not how can I get GHS compiler

Shivanand_0-1748324198100.png

 

0 Kudos
Reply
1 Reply

921 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @Shivanand,

Refer to the release notes of the BMS version you have.

There are supported compiler listed.

This is SW32K3 BMS Application AUTOSAR 4.4_R21-11 0.8.1 D2408:

danielmartynek_0-1748348259673.png

Regarding GHS compiler, please contact https://support.ghs.com/

 

Regards,

Daniel

 

0 Kudos
Reply