HVBMS EB Tresos Project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HVBMS EB Tresos Project

940件の閲覧回数
Shivanand
Contributor II

Hello @nxp

I'm trying to setup EB Tresos for HVBMS project of s32k358. In the following steps they have mentioned to add compiler path and Tresos tool path. In Compiler path it is mentioned to add GHS compiler which is commercial , can I use GNU compiler. If not how can I get GHS compiler

Shivanand_0-1748324198100.png

 

0 件の賞賛
返信
1 返信

917件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @Shivanand,

Refer to the release notes of the BMS version you have.

There are supported compiler listed.

This is SW32K3 BMS Application AUTOSAR 4.4_R21-11 0.8.1 D2408:

danielmartynek_0-1748348259673.png

Regarding GHS compiler, please contact https://support.ghs.com/

 

Regards,

Daniel

 

0 件の賞賛
返信