HSE Stream Hash with Scatter/gather input.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

HSE Stream Hash with Scatter/gather input.

1,876 次查看
phuong_nguyenle
Contributor II

My project request to stream hash with separated location of data. for secured flashing E.g:

- 1st 4bytes are in RAM 1

- 2nd 4byte are in RAM 2

- the remaining byte (is in programming sequence so that need stream Hashing) in FLASH.

 

Can I use Scatter/gather input for 1st and 2nd chunks as input in START? Then the remaining bytes shall be UPDATE later?

标记 (1)
0 项奖励
回复
2 回复数

1,848 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @phuong_nguyenle 

Yes, it is possible to use streaming and scatter/gather input at the same time.

Attached is simple demo.

However, keep in mind that there's following limitation:

image.png

And hash block size is:

 

So, each stream call requires to have data aligned to n*hash_block_size.

You can have 4 bytes on one address, next 4 bytes on second address and next data on another address. This can be covered by scatter gather. But it must be n*hash_block_size in total.

Regards,

Lukas

1,842 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

There are some troubles with the screenshot about hash block size, so I will attach it here.

0 项奖励
回复