HSE_SRV_RSP_GENERAL_ERROR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HSE_SRV_RSP_GENERAL_ERROR

935 Views
Lixinyu
Contributor I

I tried to request SHA256 hash calculation using the HSE module in the S32K312. With the RTD 3.0 package, I encountered the error code HSE_SRV_RSP_GENERAL_ERROR, but when using RTD version 2.0.3, there is no error, and the hash is correctly calculated.

Some details are as follows:

  • HSE version: HSE_FW_S32K3XX_0_2_6_0
  • RTD version: SW32K3_RTD_R21-11_3.0.0_P07_D2306
0 Kudos
Reply
1 Reply

896 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @Lixinyu 

The most common reason for this error is data cache memory. Are you sure that all the data objects used for communication with HSE are forced to non-cacheable memory? Or did you try to simply disable the data cache completely to see if it makes a difference?

Regards,

Lukas

0 Kudos
Reply