HSE Firmware install in S32k322 microcontroller .

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HSE Firmware install in S32k322 microcontroller .

285 Views
Ranjith_kumar
Contributor II

Hi NXP Support Team,

I am working on a security implementation on the S32K322 microcontroller and need to utilize the HSE (Hardware Security Engine) module for AES security operations and random number generation (TRNG).

Could you please provide:

  1. An official HSE firmware installation example project configured specifically for the S32K322 (2 MB Flash).

  2. The standard Linker Script (.ld), IVT offset, and memory boundary settings required for S32K322 HSE firmware setup.

  3. Confirmation on the exact HSE-B firmware binary package version compatible with the S32K322 derivative.

0 Kudos
Reply
2 Replies

144 Views
Ranjith_kumar
Contributor II

Hi @lukaszadrapa,

Thank you for your support. Following your guidance, I was able to install the HSE firmware successfully on my S32K322 device.

I now need to update the HSE firmware to a newer version using a new pink file, and I'm running into a problem. I based my code on the HSE firmware update flow (HSE_SRV_ID_FIRMWARE_UPDATE), and the service returns:

HSE_SRV_RSP_VERIFY_FAILED (0x55A5A164)

Setup details:
- Device:S32K322
- Firmware variant: FULL_MEM 
- Currently installed HSE FW version: Attached the image
- New pink file: Add into linker file
- Update mode: ONE_SHOT 
- Location of the new pink image: 0x00400000

Is there any example code to update the HSE firmware can you give me the guidence.

Ranjith_kumar_0-1790752089440.png

#define HSE_SRV_RSP_VERIFY_FAILED ((hseSrvResponse_t)0x55A5A164UL)

Ranjith_kumar_1-1790752155950.png

 

0 Kudos
Reply

223 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @Ranjith_kumar 

 

We provide HSE DemoExamples:

https://www.nxp.com/webapp/Download?colCode=S32K3_HSE_DemoExamples

 

It contains project S32K344_HSE_FW_INSTALL which can be quite easily ported to other S32K3 derivatives.

 

But you can use any project to install HSE firmware. It’s just necessary to do following steps:

- program HSE feature flag in OTP UTEST memory at 0x1B00_0000. This can be done either “manually” by normal flash programming (this is shown in mentioned S32K344_HSE_FW_INSTALL) or this can be done automatically by SBAF if you set FW_USAGE_FLAG_PROGRAM bit in boot configuration word. Notice that this automatic programming feature is available only on SBAF version 0.15.0 and higher. If you have some very old device, it may not work and manual programming will be required.

- program pink file somewhere to flash memory and add pointer to the pink file to IVT at offset 0x2C.  

Then just reset the MCU (2x in case of FULL_MEM firmware, 3x in case of AB_SWAP firmware) and that’s it.

 

At low level, it looks like this:

This is IVT of some application (several locations can be used, data flash is used in this case) which has FW_USAGE_FLAG_PROGRAM set and which contains pointer to FW image:

lukaszadrapa_1-1790254703462.png

 

The pink file is programmed to 0x480000:

lukaszadrapa_2-1790254714965.png

After the resets, the feature flag is automatically programmed in the UTEST and HSE firmware is installed (bit 0 in HSE GPR register at 0x4039_C028 is set):

lukaszadrapa_3-1790254752856.png

 

In the S32K344_HSE_FW_INSTALL, the feature flag is programmed by the software – see main.c file.

The pointer is added to IVT in file boot_header.c.

And pink file is linked to the project in S32K344_flash_full_mem.ld or in S32K344_flash_ab_swap.ld, depending on required configuration.

 

For details, see following resources in HSE-B firmware reference manual rev. 2.8:

Table 17. BCW content

Table 119. BCW bit mapping

Table 118. IVT structure

Table 143. Status Bits on HSE_CONFIG_GPR3 (0x4039C028)

 

How to implement it in your project if you have standard RTD project:

- open startup_cm7.s file and add pointer to pink file at offset 0x2C:

lukaszadrapa_4-1790254832253.png

 

- set bit 9 in Boot Configuration Word which is also in IVT at offset 0x4:

lukaszadrapa_5-1790254850401.png

 

- and then go to the linker file (like “linker_flash_s32k322.ld”) and link the pink file in the same way as you can see in project S32K344_HSE_FW_INSTALL.

lukaszadrapa_6-1790254941316.pnglukaszadrapa_7-1790254948399.png

 

That’s all, just build the project, load it to MCU and reset the device several times.

 

How to get latest production version of HSE firmware for S32K322:

Go to S32K3 Standard Software:

https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K3-STDSW-D

Select “Automotive SW - S32K3 - HSE Firmware”

Here search for 0.2.55.0 for S32K3x2 and S32K3x4:

lukaszadrapa_8-1790255036426.png

Download HSE_FW_S32K342_0.2.55.0_D2512.exe – this one covers also S32K322.

 

And the last thing - if you use Trace32 from Lauterbach, you can use attached script to install the firmware. It uses default location method. 

 

Regards,

Lukas

0 Kudos
Reply
%3CLINGO-SUB%20id%3D%22lingo-sub-2415877%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3EHSE%20Firmware%20install%20in%20S32k322%20microcontroller%20.%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2415877%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3EHi%20NXP%20Support%20Team%2C%3C%2FP%3E%3CP%3EI%20am%20working%20on%20a%20security%20implementation%20on%20the%20%3CSTRONG%3ES32K322%3C%2FSTRONG%3E%20microcontroller%20and%20need%20to%20utilize%20the%20HSE%20(Hardware%20Security%20Engine)%20module%20for%20AES%20security%20operations%20and%20random%20number%20generation%20(TRNG).%3C%2FP%3E%3CP%3ECould%20you%20please%20provide%3A%3C%2FP%3E%3COL%3E%3CLI%3E%3CP%3EAn%20official%20HSE%20firmware%20installation%20example%20project%20configured%20specifically%20for%20the%20%3CSTRONG%3ES32K322%3C%2FSTRONG%3E%20(2%20MB%20Flash).%3C%2FP%3E%3C%2FLI%3E%3CLI%3E%3CP%3EThe%20standard%20Linker%20Script%20(.ld)%2C%20IVT%20offset%2C%20and%20memory%20boundary%20settings%20required%20for%20S32K322%20HSE%20firmware%20setup.%3C%2FP%3E%3C%2FLI%3E%3CLI%3E%3CP%3EConfirmation%20on%20the%20exact%20HSE-B%20firmware%20binary%20package%20version%20compatible%20with%20the%20S32K322%20derivative.%3C%2FP%3E%3C%2FLI%3E%3C%2FOL%3E%3C%2FLINGO-BODY%3E%3CLINGO-SUB%20id%3D%22lingo-sub-2416136%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%20translate%3D%22no%22%3ERe%3A%20HSE%20Firmware%20install%20in%20S32k322%20microcontroller%20.%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2416136%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3EHi%26nbsp%3B%3CA%20href%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fuser%2Fviewprofilepage%2Fuser-id%2F236684%22%20target%3D%22_blank%22%3E%40Ranjith_kumar%3C%2FA%3E%26nbsp%3B%3C%2FP%3E%0A%3CBR%20%2F%3E%0A%3CP%3EWe%20provide%20HSE%20DemoExamples%3A%3C%2FP%3E%0A%3CP%3E%3CA%20href%3D%22https%3A%2F%2Fwww.nxp.com%2Fwebapp%2FDownload%3FcolCode%3DS32K3_HSE_DemoExamples%22%20target%3D%22_blank%22%20rel%3D%22nofollow%20noopener%20noreferrer%22%3Ehttps%3A%2F%2Fwww.nxp.com%2Fwebapp%2FDownload%3FcolCode%3DS32K3_HSE_DemoExamples%3C%2FA%3E%3C%2FP%3E%0A%3CBR%20%2F%3E%0A%3CP%3EIt%20contains%20project%20S32K344_HSE_FW_INSTALL%20which%20can%20be%20quite%20easily%20ported%20to%20other%20S32K3%20derivatives.%3C%2FP%3E%0A%3CBR%20%2F%3E%0A%3CP%3EBut%20you%20can%20use%20any%20project%20to%20install%20HSE%20firmware.%20It%E2%80%99s%20just%20necessary%20to%20do%20following%20steps%3A%3C%2FP%3E%0A%3CP%3E-%20program%20HSE%20feature%20flag%20in%20OTP%20UTEST%20memory%20at%200x1B00_0000.%20This%20can%20be%20done%20either%20%E2%80%9Cmanually%E2%80%9D%20by%20normal%20flash%20programming%20(this%20is%20shown%20in%20mentioned%20S32K344_HSE_FW_INSTALL)%20or%20this%20can%20be%20done%20automatically%20by%20SBAF%20if%20you%20set%20FW_USAGE_FLAG_PROGRAM%20bit%20in%20boot%20configuration%20word.%20Notice%20that%20this%20automatic%20programming%20feature%20is%20available%20only%20on%20SBAF%20version%200.15.0%20and%20higher.%20If%20you%20have%20some%20very%20old%20device%2C%20it%20may%20not%20work%20and%20manual%20programming%20will%20be%20required.%3C%2FP%3E%0A%3CP%3E-%20program%20pink%20file%20somewhere%20to%20flash%20memory%20and%20add%20pointer%20to%20the%20pink%20file%20to%20IVT%20at%20offset%200x2C.%20%26nbsp%3B%3C%2FP%3E%0A%3CP%3EThen%20just%20reset%20the%20MCU%20(2x%20in%20case%20of%20FULL_MEM%20firmware%2C%203x%20in%20case%20of%20AB_SWAP%20firmware)%20and%20that%E2%80%99s%20it.%3C%2FP%3E%0A%3CBR%20%2F%3E%0A%3CP%3EAt%20low%20level%2C%20it%20looks%20like%20this%3A%3C%2FP%3E%0A%3CP%3EThis%20is%20IVT%20of%20some%20application%20(several%20locations%20can%20be%20used%2C%20data%20flash%20is%20used%20in%20this%20case)%20which%20has%20FW_USAGE_FLAG_PROGRAM%20set%20and%20which%20contains%20pointer%20to%20FW%20image%3A%3C%2FP%3E%0A%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22lukaszadrapa_1-1790254703462.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22lukaszadrapa_1-1790254703462.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22lukaszadrapa_1-1790254703462.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F396844i8F27494EDD7C9E63%2Fimage-size%2Fmedium%3Fv%3Dv2%26amp%3Bpx%3D400%22%20role%3D%22button%22%20title%3D%22lukaszadrapa_1-1790254703462.png%22%20alt%3D%22lukaszadrapa_1-1790254703462.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FSPAN%3E%3C%2FP%3E%0A%3CBR%20%2F%3E%0A%3CP%3EThe%20pink%20file%20is%20programmed%20to%200x480000%3A%3C%2FP%3E%0A%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22lukaszadrapa_2-1790254714965.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22lukaszadrapa_2-1790254714965.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22lukaszadrapa_2-1790254714965.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F396845i2EB4308D36800E77%2Fimage-size%2Fmedium%3Fv%3Dv2%26amp%3Bpx%3D400%22%20role%3D%22button%22%20title%3D%22lukaszadrapa_2-1790254714965.png%22%20alt%3D%22lukaszadrapa_2-1790254714965.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%3EAfter%20the%20resets%2C%20the%20feature%20flag%20is%20automatically%20programmed%20in%20the%20UTEST%20and%20HSE%20firmware%20is%20installed%20(bit%200%20in%20HSE%20GPR%20register%20at%200x4039_C028%20is%20set)%3A%3C%2FP%3E%0A%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22lukaszadrapa_3-1790254752856.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22lukaszadrapa_3-1790254752856.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22lukaszadrapa_3-1790254752856.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F396846iF7837397F67211DC%2Fimage-size%2Fmedium%3Fv%3Dv2%26amp%3Bpx%3D400%22%20role%3D%22button%22%20title%3D%22lukaszadrapa_3-1790254752856.png%22%20alt%3D%22lukaszadrapa_3-1790254752856.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FSPAN%3E%3C%2FP%3E%0A%3CBR%20%2F%3E%0A%3CP%3EIn%20the%20S32K344_HSE_FW_INSTALL%2C%20the%20feature%20flag%20is%20programmed%20by%20the%20software%20%E2%80%93%20see%20main.c%20file.%3C%2FP%3E%0A%3CP%3EThe%20pointer%20is%20added%20to%20IVT%20in%20file%20boot_header.c.%3C%2FP%3E%0A%3CP%3EAnd%20pink%20file%20is%20linked%20to%20the%20project%20in%20S32K344_flash_full_mem.ld%20or%20in%20S32K344_flash_ab_swap.ld%2C%20depending%20on%20required%20configuration.%3C%2FP%3E%0A%3CBR%20%2F%3E%0A%3CP%3EFor%20details%2C%20see%20following%20resources%20in%20HSE-B%20firmware%20reference%20manual%20rev.%202.8%3A%3C%2FP%3E%0A%3CP%3ETable%2017.%E2%80%87BCW%20content%3C%2FP%3E%0A%3CP%3ETable%20119.%E2%80%87BCW%20bit%20mapping%3C%2FP%3E%0A%3CP%3ETable%20118.%E2%80%87IVT%20structure%3C%2FP%3E%0A%3CP%3ETable%20143.%E2%80%87Status%20Bits%20on%20HSE_CONFIG_GPR3%20(0x4039C028)%3C%2FP%3E%0A%3CBR%20%2F%3E%0A%3CP%3EHow%20to%20implement%20it%20in%20your%20project%20if%20you%20have%20standard%20RTD%20project%3A%3C%2FP%3E%0A%3CP%3E-%20open%20startup_cm7.s%20file%20and%20add%20pointer%20to%20pink%20file%20at%20offset%200x2C%3A%3C%2FP%3E%0A%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22lukaszadrapa_4-1790254832253.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22lukaszadrapa_4-1790254832253.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22lukaszadrapa_4-1790254832253.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F396847iEF62859842252AF5%2Fimage-size%2Fmedium%3Fv%3Dv2%26amp%3Bpx%3D400%22%20role%3D%22button%22%20title%3D%22lukaszadrapa_4-1790254832253.png%22%20alt%3D%22lukaszadrapa_4-1790254832253.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FSPAN%3E%3C%2FP%3E%0A%3CBR%20%2F%3E%0A%3CP%3E-%20set%20bit%209%20in%20Boot%20Configuration%20Word%20which%20is%20also%20in%20IVT%20at%20offset%200x4%3A%3C%2FP%3E%0A%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22lukaszadrapa_5-1790254850401.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22lukaszadrapa_5-1790254850401.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22lukaszadrapa_5-1790254850401.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F396848iF86F40ED1E89C164%2Fimage-size%2Fmedium%3Fv%3Dv2%26amp%3Bpx%3D400%22%20role%3D%22button%22%20title%3D%22lukaszadrapa_5-1790254850401.png%22%20alt%3D%22lukaszadrapa_5-1790254850401.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FSPAN%3E%3C%2FP%3E%0A%3CBR%20%2F%3E%0A%3CP%3E-%20and%20then%20go%20to%20the%20linker%20file%20(like%20%E2%80%9Clinker_flash_s32k322.ld%E2%80%9D)%20and%20link%20the%20pink%20file%20in%20the%20same%20way%20as%20you%20can%20see%20in%20project%20S32K344_HSE_FW_INSTALL.%3C%2FP%3E%0A%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22lukaszadrapa_6-1790254941316.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22lukaszadrapa_6-1790254941316.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22lukaszadrapa_6-1790254941316.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F396849i91B2D833391D314E%2Fimage-size%2Fmedium%3Fv%3Dv2%26amp%3Bpx%3D400%22%20role%3D%22button%22%20title%3D%22lukaszadrapa_6-1790254941316.png%22%20alt%3D%22lukaszadrapa_6-1790254941316.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FSPAN%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22lukaszadrapa_7-1790254948399.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22lukaszadrapa_7-1790254948399.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22lukaszadrapa_7-1790254948399.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F396850i75EBD42F51229EBA%2Fimage-size%2Fmedium%3Fv%3Dv2%26amp%3Bpx%3D400%22%20role%3D%22button%22%20title%3D%22lukaszadrapa_7-1790254948399.png%22%20alt%3D%22lukaszadrapa_7-1790254948399.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FSPAN%3E%3C%2FP%3E%0A%3CBR%20%2F%3E%0A%3CP%3EThat%E2%80%99s%20all%2C%20just%20build%20the%20project%2C%20load%20it%20to%20MCU%20and%20reset%20the%20device%20several%20times.%3C%2FP%3E%0A%3CBR%20%2F%3E%0A%3CP%3EHow%20to%20get%20latest%20production%20version%20of%20HSE%20firmware%20for%20S32K322%3A%3C%2FP%3E%0A%3CP%3EGo%20to%20S32K3%20Standard%20Software%3A%3C%2FP%3E%0A%3CP%3E%3CA%20href%3D%22https%3A%2F%2Fwww.nxp.com%2Fwebapp%2Fswlicensing%2Fsso%2FdownloadSoftware.sp%3Fcatid%3DSW32K3-STDSW-D%22%20target%3D%22_blank%22%20rel%3D%22nofollow%20noopener%20noreferrer%22%3Ehttps%3A%2F%2Fwww.nxp.com%2Fwebapp%2Fswlicensing%2Fsso%2FdownloadSoftware.sp%3Fcatid%3DSW32K3-STDSW-D%3C%2FA%3E%3C%2FP%3E%0A%3CP%3ESelect%20%E2%80%9CAutomotive%20SW%20-%20S32K3%20-%20HSE%20Firmware%E2%80%9D%3C%2FP%3E%0A%3CP%3EHere%20search%20for%200.2.55.0%20for%20S32K3x2%20and%20S32K3x4%3A%3C%2FP%3E%0A%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22lukaszadrapa_8-1790255036426.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22lukaszadrapa_8-1790255036426.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22lukaszadrapa_8-1790255036426.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F396851i3FF86F15238EACCC%2Fimage-size%2Fmedium%3Fv%3Dv2%26amp%3Bpx%3D400%22%20role%3D%22button%22%20title%3D%22lukaszadrapa_8-1790255036426.png%22%20alt%3D%22lukaszadrapa_8-1790255036426.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%3EDownload%20HSE_FW_S32K342_0.2.55.0_D2512.exe%20%E2%80%93%20this%20one%20covers%20also%20S32K322.%3C%2FP%3E%0A%3CBR%20%2F%3E%0A%3CP%3EAnd%20the%20last%20thing%20-%20if%20you%20use%20Trace32%20from%20Lauterbach%2C%20you%20can%20use%20attached%20script%20to%20install%20the%20firmware.%20It%20uses%20default%20location%20method.%26nbsp%3B%3C%2FP%3E%0A%3CBR%20%2F%3E%0A%3CP%3ERegards%2C%3C%2FP%3E%0A%3CP%3ELukas%3C%2FP%3E%3C%2FLINGO-BODY%3E%3CLINGO-SUB%20id%3D%22lingo-sub-2417368%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%20translate%3D%22no%22%3ERe%3A%20HSE%20Firmware%20install%20in%20S32k322%20microcontroller%20.%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2417368%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3EHi%20%3CA%20href%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fuser%2Fviewprofilepage%2Fuser-id%2F37795%22%20target%3D%22_blank%22%3E%40lukaszadrapa%3C%2FA%3E%2C%3C%2FP%3E%3CP%3EThank%20you%20for%20your%20support.%20Following%20your%20guidance%2C%20I%20was%20able%20to%20install%20the%20HSE%20firmware%20successfully%20on%20my%20S32K322%20device.%3C%2FP%3E%3CP%3EI%20now%20need%20to%20update%20the%20HSE%20firmware%20to%20a%20newer%20version%20using%20a%20new%20pink%20file%2C%20and%20I'm%20running%20into%20a%20problem.%20I%20based%20my%20code%20on%20the%20HSE%20firmware%20update%20flow%20(HSE_SRV_ID_FIRMWARE_UPDATE)%2C%20and%20the%20service%20returns%3A%3C%2FP%3E%3CP%3EHSE_SRV_RSP_VERIFY_FAILED%20(0x55A5A164)%3C%2FP%3E%3CP%3ESetup%20details%3A%3CBR%20%2F%3E-%20Device%3AS32K322%3CBR%20%2F%3E-%20Firmware%20variant%3A%20FULL_MEM%26nbsp%3B%3CBR%20%2F%3E-%20Currently%20installed%20HSE%20FW%20version%3A%20Attached%20the%20image%3CBR%20%2F%3E-%20New%20pink%20file%3A%20Add%20into%20linker%20file%3CBR%20%2F%3E-%20Update%20mode%3A%20ONE_SHOT%26nbsp%3B%3CBR%20%2F%3E-%20Location%20of%20the%20new%20pink%20image%3A%200x00400000%3CBR%20%2F%3E%3CBR%20%2F%3E%3C%2FP%3E%3CP%3EIs%20there%20any%20example%20code%20to%20update%20the%20HSE%20firmware%20can%20you%20give%20me%20the%20guidence.%3C%2FP%3E%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22Ranjith_kumar_0-1790752089440.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22Ranjith_kumar_0-1790752089440.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F397074i5780BC1B2E5734D9%2Fimage-size%2Fmedium%3Fv%3Dv2%26amp%3Bpx%3D400%22%20role%3D%22button%22%20title%3D%22Ranjith_kumar_0-1790752089440.png%22%20alt%3D%22Ranjith_kumar_0-1790752089440.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%3CP%3E%23define%20HSE_SRV_RSP_VERIFY_FAILED%20((hseSrvResponse_t)0x55A5A164UL)%3C%2FP%3E%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%22Ranjith_kumar_1-1790752155950.png%22%20style%3D%22width%3A%20400px%3B%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22Ranjith_kumar_1-1790752155950.png%22%20style%3D%22width%3A%20384px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F397075i7DB6476721862A1E%2Fimage-size%2Fmedium%3Fv%3Dv2%26amp%3Bpx%3D400%22%20role%3D%22button%22%20title%3D%22Ranjith_kumar_1-1790752155950.png%22%20alt%3D%22Ranjith_kumar_1-1790752155950.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%3CBR%20%2F%3E%3C%2FLINGO-BODY%3E