HSE DATA FLASH Usage

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,891件の閲覧回数
S3RD4R
Contributor I

Hi all,

In the Crypto_SymmetricPrimitives example's linker file, it says "Last 128 KB of DATA_FLASH reserved by HSE Firmware (not supported in this linker file)".

My MCU is s32k344 and it has a data flash of 128KB. If this is true, when HSE is enabled in any application, i can not use data flash? I was hopng to store some of my parameters in data flash and i am also using HSE.

I am confused about this. Any help will be appreciated.

Thank you,

 

0 件の賞賛
返信
1 解決策
1,822件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

In reference manual in the application boot chapter you will see which memories are available for application:

In case HSE is enabled it will take a small portion of Data flash and for application will be still available 88KB.

petervlna_0-1695803815898.png

Best regards,

Peter

 

 

 

元の投稿で解決策を見る

1 返信
1,823件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

In reference manual in the application boot chapter you will see which memories are available for application:

In case HSE is enabled it will take a small portion of Data flash and for application will be still available 88KB.

petervlna_0-1695803815898.png

Best regards,

Peter