Gmac_IP_InitDMA returns GMAC_STATUS_TIMEOUT

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Gmac_IP_InitDMA returns GMAC_STATUS_TIMEOUT

跳至解决方案
3,994 次查看
the_chuck77
Contributor II

Hi,

 

I am trying to initialize the Gmac on the s32k324.

I am basing my program off of the example code "MR_CANHUB3_IEEE1722", which runs fine on our s32k344 demo board.

When initializing the Gmac, it is getting stuck in a do()-while loop after attempting to provide a software reset (lines 405-414):

the_chuck77_0-1710779376105.png

I have configured all of the proper pins to have their respective GMAC uses. As well as ensured the driver configurations are the same as in the example project.

 

I am not sure what I am doing wrong to cause this to not succeed, does anyone have any advice?

 

 

0 项奖励
回复
1 解答
3,968 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

it can be due to the S32K3 EMAC lacks of RMII reference clock. It should be provided by the external PHY/MAC chip or external clock (50MHz) after power up. Please check this clock on your board, to be sure of correct connection between S32K3 RMII reference clock pin and the clock source.

BR, Petr

在原帖中查看解决方案

2 回复数
3,969 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

it can be due to the S32K3 EMAC lacks of RMII reference clock. It should be provided by the external PHY/MAC chip or external clock (50MHz) after power up. Please check this clock on your board, to be sure of correct connection between S32K3 RMII reference clock pin and the clock source.

BR, Petr

3,964 次查看
the_chuck77
Contributor II

This was the issue, our PHY was not outputting the reference clock prior to attempting to initialize.

0 项奖励
回复