Global Pin Control Low / High Register Global Interrupt Control Low /High Register

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Global Pin Control Low / High Register Global Interrupt Control Low /High Register

2,338件の閲覧回数
641705644
Contributor II

hello anyone,

   I'm looking at s32k RM, could anyone tell me how to use  Global Pin Control Low / High Register and  Global Interrupt Control Low /High Register in S32k MCU, I means how work this register. thanks.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,192件の閲覧回数
641705644
Contributor II

these are descripted in section "12.7 Functional description" in S32K1xx Series Reference Manual

0 件の賞賛
返信

2,192件の閲覧回数
641705644
Contributor II

I known, due to my poor English, I do not understand that section correctly. after reading the whole chapter, I understand. the Global Pin Control Low / High Register can update lower 16bit of 32 PCRs (PORT_PCR[0-31])  with the same value. the higher 16 bit of Global Pin Control Low / High Register select which PCRs are updated. the value in the lower 16 bit of Global Pin Control Low / High Register are updated to the lower 16bits of the selcted PCRs.  in the similar way, Global Interrupt Control Low /High Register update the higher 16bits of the PCRs.

0 件の賞賛
返信