Gibberish receiving when transmitting custom etherType Ethernet Frame

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Gibberish receiving when transmitting custom etherType Ethernet Frame

跳至解决方案
163 次查看
R_S002
Contributor III

Hello @PavelL and NXP Community,

I'm sending Ethernet frames with a custom EtherType (0xA5A5) between S32K344 and TJA1103 connected via media converters. I have run and tested LWIP_S32K344 on the same hardware, and it works flawlessly. Below, I have mentioned the transmission code, as well as the frames received on Wireshark. 

/*
 * tx_eth_udp.c
 *
 * Purpose: Build and transmit a valid Ethernet -> IPv4 -> UDP frame
 * Platform: S32K344 + TJA1103 (RMII)
 * Author: RohanS002 Gettobyte
 * Date: 11-Oct-2025
 */
 
#include "Mcal.h"
#include "Clock_Ip.h"
#include "Siul2_Port_Ip_Cfg.h"
#include "Siul2_Port_Ip.h"
#include "Gmac_Ip.h"
#include "string.h"
#include "stdint.h"
#include "stdbool.h"
 
/* ===== app control ===== */
volatile int exit_code = 0;
 
/* ===== GMAC/PHY globals ===== */
#define INST_GMAC_0     (0U)
Gmac_Ip_StatusType Status = 0;
 
/* Replace with your actual MACs for both boards */
static uint8 MacAddr_Src[6U] = { 0x10, 0x11, 0x22, 0x77, 0x77, 0x77 }; /* this board */
static uint8 MacAddr_Dest[6U] = { 0x10, 0x11, 0x22, 0x77, 0x77, 0x78 }; /* peer board */
 
/* ===== PHY discovery scratch ===== */
static uint16 phy_addr; /* discovered PHY address (0..31) */
static uint16 register_value_0;
static uint16 register_value_1;
 
/* ===== TX structures ===== */
static Gmac_Ip_BufferType TxBuffer = { 0 };
static Gmac_Ip_TxInfoType TxInfo = { 0 };
static Gmac_Ip_TxOptionsType TxOptions = {
TRUE, /* add CRC/FCS and pad in hardware */
GMAC_CRC_AND_PAD_INSERTION, GMAC_CHECKSUM_INSERTION_PROTO_PSEUDOH /* we compute checksums in software */
};
 
/* ====== Simple busy-wait delay (approx) ====== */
/* Adjust for your clock; this is just to pace packets for Wireshark */
static void delay_cycles(volatile uint32_t cycles) {
while (cycles--) {
__asm("nop");
}
}
 
/*
 * Ethernet Frame Format (IEEE 802.3 / Ethernet II)
 *
 * +------------+------------+-----------+------------------+-----------+
 * | Destination|   Source   | EtherType |      Payload     |    FCS    |
 * |   MAC (6B) |   MAC (6B) |   (2B)    |    (46–1500 B)   |   (4B)    |
 * +------------+------------+-----------+------------------+-----------+
 *
 * Field Details:
 * - Destination MAC (6 bytes): Who the frame is sent to
 * - Source MAC      (6 bytes): Who is sending the frame
 * - EtherType/Length(2 bytes): Protocol indicator
 * e.g. 0x0800 = IPv4, 0x0806 = ARP, custom = 0x88B5 etc.
 * - Payload         (46–1500 bytes): Actual data being sent
 * - FCS             (4 bytes): CRC checksum (auto-inserted by GMAC HW)
 *
 * In our code:
 * [0..5]   -> txFrame.dstMac
 * [6..11]  -> txFrame.srcMac
 * [12..13] -> txFrame.etherType
 * [14..N]  -> txFrame.payload
 * [N+1..]  -> FCS (handled automatically by hardware)
 */
 
/* A structure to represent an Ethernet frame in a user-friendly way. */
typedef struct {
uint8 dstMac[6];
uint8 srcMac[6];
uint16 etherType;
uint8 payload[64]; /* A buffer for the payload data. */
uint16 payloadLen; /* The actual length of the payload. */
} EthFrame_t;
 
/**
 * @brief Constructs a raw Ethernet frame into a GMAC hardware buffer.
 * @param txBuf A pointer to the GMAC transmit buffer where the frame will be built.
 * @param frame A pointer to the user-friendly frame structure containing the data.
 */
static void BuildEthernetFrame(Gmac_Ip_BufferType *txBuf,
const EthFrame_t *frame) {
/* Get a pointer to the beginning of the hardware buffer's data area. */
uint8 *ptr = txBuf->Data;
 
/* Copy the 6-byte destination MAC address into the buffer. */
memcpy(ptr, frame->dstMac, 6U);
ptr += 6U; // Move the pointer forward by 6 bytes.
 
/* Copy the 6-byte source MAC address. */
memcpy(ptr, frame->srcMac, 6U);
ptr += 6U; // Move the pointer forward.
 
/* Copy the 2-byte EtherType, handling big-endian byte order manually. */
*ptr++ = (uint8) ((frame->etherType >> & 0xFFU); // Most Significant Byte (MSB)
*ptr++ = (uint8) (frame->etherType & 0xFFU); // Least Significant Byte (LSB)
 
/* Copy the payload data into the buffer. */
memcpy(ptr, frame->payload, frame->payloadLen);
ptr += frame->payloadLen; // Move the pointer past the payload.
 
/* Set the total length of the buffer. The FCS (CRC) will be added by the hardware. */
txBuf->Length = (uint32) (ptr - txBuf->Data);
}
 
/* ====== PHY init (TJA110x via MDIO) ====== */
static void Eth_Phy_Init(void) {
/* Enable MDIO (Management Data I/O) for PHY communication */
Gmac_Ip_EnableMDIO(INST_GMAC_0, FALSE, 48000000U);
 
/* --- Discover PHY address by reading PHY ID1/ID2 --- */
for (phy_addr = 0U; phy_addr < 32U; ++phy_addr) {
(void) Gmac_Ip_MDIORead(INST_GMAC_0, phy_addr, 2U, &register_value_0,
1U);
(void) Gmac_Ip_MDIORead(INST_GMAC_0, phy_addr, 3U, &register_value_1,
1U);
 
/* TJA110x ID: 0x001B / 0xB013 (adjust if your silicon differs) */
if ((register_value_0 == 0x001B) && (register_value_1 == 0xB013)) {
break;
}
}
 
/* Reset PHY */
(void) Gmac_Ip_MDIOWrite(INST_GMAC_0, phy_addr, 0U, 0x8000U, 1U);
/* Wait for reset done (bit15 clears) */
do {
(void) Gmac_Ip_MDIORead(INST_GMAC_0, phy_addr, 0U, &register_value_0,
1U);
} while (register_value_0 & 0x8000U);
 
/* Basic sanity checks (optional but good while bringing up) */
/* ePHY enable check */
(void) Gmac_Ip_MDIOReadMMD(INST_GMAC_0, phy_addr, 1, 0x8048U,
&register_value_0, 1U);
/* master/slave */
(void) Gmac_Ip_MDIOReadMMD(INST_GMAC_0, phy_addr, 1, 0x0834U,
&register_value_0, 1U);
/* xMII config (Rev-RMII) */
(void) Gmac_Ip_MDIOReadMMD(INST_GMAC_0, phy_addr, 30, 0xAFC6U,
&register_value_0, 1U);
 
/* Link status poll (bit2 of 0x8102) */
do {
(void) Gmac_Ip_MDIOReadMMD(INST_GMAC_0, phy_addr, 30, 0x8102U,
&register_value_0, 1U);
} while (((register_value_0 & (1U << 2)) == 0U));
}
 
/* ====== Main ====== */
int main(void) {
/* Put MAC into RMII mode through DCM (per your original code) */
IP_DCM_GPR->DCMRWF1 = (IP_DCM_GPR->DCMRWF1
& ~DCM_GPR_DCMRWF1_MAC_CONF_SEL_MASK)
| DCM_GPR_DCMRWF1_MAC_CONF_SEL(2U);
 
/* Clocks / Pins / GMAC driver (generated by RTD config tool) */
Clock_Ip_Init(&Clock_Ip_aClockConfig[0]);
Siul2_Port_Ip_Init(
NUM_OF_CONFIGURED_PINS_PortContainer_0_BOARD_InitPeripherals,
g_pin_mux_InitConfigArr_PortContainer_0_BOARD_InitPeripherals);
 
Status = Gmac_Ip_Init(INST_GMAC_0, &Gmac_0_ConfigPB);
DevAssert(Status == GMAC_STATUS_SUCCESS);
 
/* Bring up PHY and wait for link */
Eth_Phy_Init();
 
/* Declare a local variable to hold the Ethernet frame data. */
EthFrame_t txFrame;
 
/* --- Assemble the Ethernet Frame --- */
/* Copy the retrieved hardware MAC as the source address. */
memcpy(txFrame.srcMac, MacAddr_Src, 6U);
/* Copy the predefined destination MAC address. */
memcpy(txFrame.dstMac, MacAddr_Dest, 6U);
/* Set a custom EtherType (e.g., for a proprietary protocol). 0xBB80 = 48000 */
txFrame.etherType = 0xA5A5U;
/* Set the payload length. Ethernet requires a minimum frame size, so payloads < 46 bytes get padded. */
txFrame.payloadLen = 46U;
 
/* Fill the payload with dummy data (a simple ascending sequence of numbers). */
for (uint16 i = 0; i < txFrame.payloadLen; i++) {
txFrame.payload[i] = (uint8) i;
}
 
/* --- Prepare for Transmission --- */
/* Request a free transmit buffer from the GMAC driver's internal queue. */
Status = Gmac_Ip_GetTxBuff(INST_GMAC_0, 0U, &TxBuffer, NULL_PTR);
DevAssert(Status == GMAC_STATUS_SUCCESS); // Halt if no buffer is available.
 
/* Call the helper function to copy the assembled frame into the hardware buffer. */
BuildEthernetFrame(&TxBuffer, &txFrame);
 
/* ==== Send once per second so Wireshark is easy to read ==== */
for (;;) {
 
/* --- Send the Frame --- */
/* Instruct the GMAC hardware to send the contents of the buffer. */
Status = Gmac_Ip_SendFrame(INST_GMAC_0, 0U, &TxBuffer, &TxOptions);
DevAssert(Status == GMAC_STATUS_SUCCESS); // Halt if sending fails.
 
/* Wait for the frame to be transmitted */
do {
Status = Gmac_Ip_GetTransmitStatus(INST_GMAC_0, 0U, &TxBuffer,
&TxInfo);
} while (Status == GMAC_STATUS_BUSY);
 
DevAssert((GMAC_STATUS_SUCCESS == Status) || (0U != TxInfo.ErrMask));
 
/* ~1 second delay (tune for your clock: this is a rough software wait) */
delay_cycles(10000000U);
 
if (exit_code != 0) {
break;
}
}
 
return exit_code;
}

 

标记 (2)
0 项奖励
回复
1 解答
146 次查看
PavelL
NXP Employee
NXP Employee

Hello @R_S002 ,

I believe that this code row:

*ptr++ = (uint8) ((frame->etherType >> & 0xFFU); // Most Significant Byte (MSB)
 
should look like:

*ptr++ = (uint8)((frame->etherType >> 8 ) & 0xFFU); // Most Significant Byte (MSB)
 

Best regards,

Pavel

在原帖中查看解决方案

0 项奖励
回复
1 回复
147 次查看
PavelL
NXP Employee
NXP Employee

Hello @R_S002 ,

I believe that this code row:

*ptr++ = (uint8) ((frame->etherType >> & 0xFFU); // Most Significant Byte (MSB)
 
should look like:

*ptr++ = (uint8)((frame->etherType >> 8 ) & 0xFFU); // Most Significant Byte (MSB)
 

Best regards,

Pavel

0 项奖励
回复