Getting wrong value of cell 14 and stack voltage when using FRDM33771B and S32k144

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Getting wrong value of cell 14 and stack voltage when using FRDM33771B and S32k144

2,462件の閲覧回数
Shobha
Contributor I

Hello,

I have interfaced mc33771 with S32K144 and used 7 cells. I have done the cell tapping as per the given connection in datasheet given for cells less than 14. I'm getting wrong value of cell 14 and total stack voltage. I am not able to get why is this happening. Also I'm getting FAULT1 and FAULT3 as yes. How can I know what's this fault is for? I've attached the snip below
It would be great if you can help me with this.

Thanks in advance!

cells_snip2.PNGcells_snip2.PNG

 

afterchange1.PNGafterchange1.PNG

 

0 件の賞賛
返信
5 返答(返信)

2,224件の閲覧回数
Gad_usr1
Contributor II

Hi, were you able to solve this issue?

0 件の賞賛
返信

2,416件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

HI 

Please install 14 cells for this HW/SW,if less than 14 cells the hardware also need update.

0 件の賞賛
返信

2,410件の閲覧回数
Shobha
Contributor I

Hey
Can you pl elaborate on how to install 14 cells for this HW/SW, if less than 14 cells.

0 件の賞賛
返信

2,397件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

You can down AN12536 for getting more information.

0 件の賞賛
返信

2,393件の閲覧回数
Shobha
Contributor I

Yes I've already downloaded AN12536 and done the connection of 7 cells as per the Type A wiring shown. Below is the attached connection that I've followed.

cell_connection.PNGcell_connection.PNG

0 件の賞賛
返信