Get SDID value for S32K118EVB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Get SDID value for S32K118EVB

1,377件の閲覧回数
rahulpkumar-2612
Contributor II

Hi,

I am using S32K118EVB and need to get SDID details. I found the below lines of code in the project i am using:

/* SDID Bit Fields */
#define SIM_SDID_FEATURES_MASK 0xFFu
#define SIM_SDID_FEATURES_SHIFT 0u
#define SIM_SDID_FEATURES_WIDTH 8u
#define SIM_SDID_FEATURES(x) (((uint32_t)(((uint32_t)(x))<<SIM_SDID_FEATURES_SHIFT))&SIM_SDID_FEATURES_MASK)
#define SIM_SDID_PACKAGE_MASK 0xF00u
#define SIM_SDID_PACKAGE_SHIFT 8u
#define SIM_SDID_PACKAGE_WIDTH 4u
#define SIM_SDID_PACKAGE(x) (((uint32_t)(((uint32_t)(x))<<SIM_SDID_PACKAGE_SHIFT))&SIM_SDID_PACKAGE_MASK)
#define SIM_SDID_REVID_MASK 0xF000u
#define SIM_SDID_REVID_SHIFT 12u
#define SIM_SDID_REVID_WIDTH 4u
#define SIM_SDID_REVID(x) (((uint32_t)(((uint32_t)(x))<<SIM_SDID_REVID_SHIFT))&SIM_SDID_REVID_MASK)
#define SIM_SDID_RAMSIZE_MASK 0xF0000u
#define SIM_SDID_RAMSIZE_SHIFT 16u
#define SIM_SDID_RAMSIZE_WIDTH 4u
#define SIM_SDID_RAMSIZE(x) (((uint32_t)(((uint32_t)(x))<<SIM_SDID_RAMSIZE_SHIFT))&SIM_SDID_RAMSIZE_MASK)
#define SIM_SDID_DERIVATE_MASK 0xF00000u
#define SIM_SDID_DERIVATE_SHIFT 20u
#define SIM_SDID_DERIVATE_WIDTH 4u
#define SIM_SDID_DERIVATE(x) (((uint32_t)(((uint32_t)(x))<<SIM_SDID_DERIVATE_SHIFT))&SIM_SDID_DERIVATE_MASK)
#define SIM_SDID_SUBSERIES_MASK 0xF000000u
#define SIM_SDID_SUBSERIES_SHIFT 24u
#define SIM_SDID_SUBSERIES_WIDTH 4u
#define SIM_SDID_SUBSERIES(x) (((uint32_t)(((uint32_t)(x))<<SIM_SDID_SUBSERIES_SHIFT))&SIM_SDID_SUBSERIES_MASK)
#define SIM_SDID_GENERATION_MASK 0xF0000000u
#define SIM_SDID_GENERATION_SHIFT 28u
#define SIM_SDID_GENERATION_WIDTH 4u
#define SIM_SDID_GENERATION(x) (((uint32_t)(((uint32_t)(x))<<SIM_SDID_GENERATION_SHIFT))&SIM_SDID_GENERATION_MASK)

 

How do I use these functions to get the version details? Could you please suggest which one to use and what needs to be passed as the argument 'x'?

I need the details so that I can transmit the same serially for the project our team is working on.

Thank you in advance!

0 件の賞賛
返信
1 返信

1,368件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi rahulpkumar,

Please read the S32K1xx MCU Family - Reference Manual for more detail about SDID:

11.3.1.8 System Device Identification Register (SDID).png11.3.1.8 System Device Identification Register (SDID) FEATURES.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信