Generating makefiles from S32Studio

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Generating makefiles from S32Studio

跳至解决方案
1,934 次查看
KADEL
Contributor I

How can I generate makefiles from my  C project in S32studio. 

NOTE: the option of "automatically generate make files" is dimmed and not working

EXAMPLE1.PNG

 

0 项奖励
回复
1 解答
1,890 次查看
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @KADEL , 

 

Apologies for replying late. 

 

As I looked in the build properties, I see that by default the selection is "external builder" as shown below

 

Mehul_Patel_NXP_0-1691784480831.png

 

You have selected "internal builder" for you project. I can see that when internal builder is selected it disables the ""Generate makefiles automatically" 

 

Please can you check if it works with by default option that is "external builder". 

 

Also, if you have selected internal builder for some reason, or anything which is changing the particular option, please can you explain the requirement. 

 

Thank you. Kind regards. 

 

- Mehul Patel

 

 

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,744 次查看
KADEL
Contributor I

Hello @Mehul_Patel_NXP ,

Thank you for replying.

Unfortunately, also the choice of Internal build is dimmed, so I can't change it to an external builder. 

I tried the "Restore Defaults" option but the internal builder remains the same and dimmed. as shown in the screenshot. 

Thank you.

0 项奖励
回复
1,891 次查看
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @KADEL , 

 

Apologies for replying late. 

 

As I looked in the build properties, I see that by default the selection is "external builder" as shown below

 

Mehul_Patel_NXP_0-1691784480831.png

 

You have selected "internal builder" for you project. I can see that when internal builder is selected it disables the ""Generate makefiles automatically" 

 

Please can you check if it works with by default option that is "external builder". 

 

Also, if you have selected internal builder for some reason, or anything which is changing the particular option, please can you explain the requirement. 

 

Thank you. Kind regards. 

 

- Mehul Patel

 

 

0 项奖励
回复
1,804 次查看
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @KADEL , 

Is this problem is solved? Do you have any further issue. 

Please kindly let us know. 

Thank you. 

0 项奖励
回复