GPIO digital filter

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GPIO digital filter

6,032件の閲覧回数
eduardplanas
Contributor I

I'm trying to configure in a S32K146 the digital filter function for the input pins, but I can not see any result. Is there more information about this function than the included in the Reference Manual?

Thank you,

Eduard.

0 件の賞賛
返信
6 返答(返信)

5,100件の閲覧回数
muellermathias
Contributor III

@danielmartynek 

Is there (more) detailed information about how the filter works internally / which kind of filter is used?

E.g. the sentence "Configures the maximum size of the glitches, in clock cycles, that the digital filter absorbs for the enabled digital filters" regarding DFWR in the Reference Manual is not very illustrative (at least not to me).

What exactly are "glitches" in this case and how are they "absorbed" by the filter?

Thank you in advance!

0 件の賞賛
返信

5,083件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @muellermathias,

It is just a simple digital filter.

danielmartynek_0-1649337302855.png

Let's say there is a stable logic HIGH at the input.

If the digital filter is anabled, the Filter Length defines how long the input signal must be driven LOW before the MCU detects the falling edge.

Pulses that are shorter are absorbed.

I need to mention that the accuracy of the filter depends on the accuracy of the clock selected for the filter.

 

Regards,

Daniel

 

 

5,646件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

Did you follow the configuration sequence in Section 12.1.3, RM r.8?

Can you share your code?

Regards,

Daniel 

0 件の賞賛
返信

5,646件の閲覧回数
eduardplanas
Contributor I

Hi,

I followed the configuration sequence from section 11.1.3 (Digital input filter configuration sequence).

First of all I configured the pins through the function PINS_DRV_Init, then I write direct to the registers as follow:

PINS_DRV_Init(NUM_OF_CONFIGURED_PINS, g_pin_mux_InitConfigArr);

PORTB->DFCR = PORT_DFCR_CS(PORT_DIGITAL_FILTER_LPO_CLOCK);
PORTB->DFWR = PORT_DFWR_FILT(0x1F);
PORTB->DFER |= 1<<23;
PORTB->PCR[23] &= ~0x700;
PORTB->PCR[23] |= 0x100;
DelayFilter=0; while(DelayFilter<TIME_DELAY_FILTER) DelayFilter++;
PORTB->PCR[23] &= ~0x700;
PORTB->PCR[23] |= 0x100;

PORTC->DFCR = PORT_DFCR_CS(PORT_DIGITAL_FILTER_LPO_CLOCK);
PORTC->DFWR = PORT_DFWR_FILT(0x1F);
PORTC->DFER |= 1<<14;
PORTC->PCR[14] &= ~0x700;
PORTC->PCR[14] |= 0x100;
DelayFilter=0; while(DelayFilter<TIME_DELAY_FILTER) DelayFilter++;

PORTC->PCR[14] &= ~0x700;
PORTC->PCR[14] |= 0x100;

PORTC->DFCR = PORT_DFCR_CS(PORT_DIGITAL_FILTER_LPO_CLOCK);
PORTC->DFWR = PORT_DFWR_FILT(0x1F);
PORTC->DFER |= 1<<15;
PORTC->PCR[15] &= ~0x700;
PORTC->PCR[15] |= 0x100;
DelayFilter=0; while(DelayFilter<TIME_DELAY_FILTER) DelayFilter++;

PORTC->PCR[15] &= ~0x700;
PORTC->PCR[15] |= 0x100;

Regards,

Eduard.

0 件の賞賛
返信

5,646件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Eduard, 

Can you use the below code?

It does filter glitches.

void PORTD_IRQHandler(void)
{
  __asm__("BKPT");
  PORTD->ISFR = 0x10;
}

int main(void)
{
  PCC->PCCn[PCC_PORTD_INDEX]|= PCC_PCCn_CGC_MASK; /* Enable clock for PORTD */
  PORTD->PCR[4] |= PORT_PCR_MUX(1) | PORT_PCR_IRQC(9);
  /* Port D4: MUX = ALT1, GPIO
  * ISF flag and Interrupt when logic 1
  **/

  S32_NVIC->ISER[1] = (1 << (62 % 32)); // PORTD interrupt
  S32_NVIC->IP[62] = 0x00;              // PORTD Interrupt Priority level 0

  PORTD->DFWR = 0x1F;       // FILT = 31
  PORTD->DFCR = 1;          // CS = 1 Digital filters are clocked by the LPO clock.
  PORTD->DFER = 0x00000010; // PTD4

  while(1)
  {
  }
}‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

Regards,

Daniel

0 件の賞賛
返信

5,646件の閲覧回数
eduardplanas
Contributor I

Hi Daniel,

I will use it, thank you very much,

Eduard.

0 件の賞賛
返信