GPIO Interrupt Handler

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GPIO Interrupt Handler

1,180件の閲覧回数
kesanli_cinci
Contributor I

Hello, 

I configured a GPIO as an interrupt and wrote a callback function for this GPIO. 

At the end of the callback function, interrupt flag is cleared. Inside this callback function, a task is notified. Before jumping to the task, interrupt flag is cleared at the the end of the callback function. 

However, I use this GPIO's status (HIGH, LOW) in order to read some registers in the task. Because I clear interrupt, I am not able to read this pin as HIGH. Operating system is FreeRTOS. That's why, I can not put this read operation inside Callback function because I use SPI_send function in this read operation.

 

How can I make read operation without clearing the interrupt flag? 

 

 

 

 

0 件の賞賛
返信
1 返信

1,157件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

could you please describe your intention in more details, maybe share piece of code you have?
Also what S32K1 device and RTD version is used in fact?
You should be able to read pin status/level at any time using Gpio_Dio_Ip_ReadPin function.
 
BR, Petr
0 件の賞賛
返信