GDB PEMicro debugging Interface not listed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

GDB PEMicro debugging Interface not listed

4,410 次查看
rahulpkumar-2612
Contributor II

Hi,

I am using S32DS for platform with S32K118 EVB. I have installed GDM PEMicro debugging interface and trying to use the Open SDA USB for connection.

But the PEMicro interface is not listed in the tool chain. 

For flashing an application to the board, how do I select the tool?

I tried S32DS for ARM2.2 to build a program and the PEMicro tool was available n it. I tried copying the srec file)of an available project) to the EVB drive, and the Green LED near to the SDA USB port started blinking. But the same was not possible with S32DS for platforms as the tool was not listed. Is it not supported?

Does it have anything to do with the system I am using (Windows 10)?

Please advise.

Screenshots attached for reference.

0 项奖励
回复
3 回复数

4,401 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Have you select the "GDB PEMicro Debugging Interface" when create new project?

Debugger GDB PEMicro Deubgging Interface.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

4,395 次查看
rahulpkumar-2612
Contributor II

Hello Robin,

Yes I did select the option while creating the project.

标记 (1)
0 项奖励
回复

4,386 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

How do you installed GDM PEMicro debugging interface? The version of GNU ARM PEMicro Interface Debugging Support on my S32DS3.4 was 5.1.4. But you are showing version 5.1.7.

GNU ARM PEMicro Interface Debugging Support.png

Have you tried uninstall the S32DS and install it again? 

0 项奖励
回复