Functional Safety Compilers for S32K3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Functional Safety Compilers for S32K3

1,641件の閲覧回数
m87
Contributor I

We highly rely on NXPs AUTOSAR Real Time Drivers (RTDs) and other tools and framework (like SPD or SCST). NXP gives support to a number of compilers (NXP-GCC, IAR, DIAB and GHS) but we wish to use (Arm Compiler for Embedded FuSa) which is not in the last. 


1.                  Are there any ongoing efforts between NXP and ARM to add the ARM compiler to the list of compilers?  

2.                  Would NXP offer any technical support to help migrate from NXP GCC based compiler to the AMR Clang based compiler? For example re-run the unit tests for the RTDs or other tools using the new complier (with NXPs recommended options)? 


(https://developer.arm.com/Tools%20and%20Software/Arm%20Compiler%20for%20Embedded%20FuSa). 

タグ(2)
0 件の賞賛
返信
1 返信

1,613件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

1. Are there any ongoing efforts between NXP and ARM to add the ARM compiler to the list of compilers?

No. At least I am not aware of any as NXP added GCC support and GHS+IAR are supported from historic reasons.

2. Would NXP offer any technical support to help migrate from NXP GCC based compiler to the AMR Clang based compiler? For example re-run the unit tests for the RTDs or other tools using the new complier (with NXPs recommended options)?

Not sure here. Best is to rise a request at paid support:

https://www.nxp.com/support/support/nxp-engineering-services:SW-SUPPORT

Best regards,

Peter

0 件の賞賛
返信