Functional Safety Compilers for S32K3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Functional Safety Compilers for S32K3

1,599 Views
m87
Contributor I

We highly rely on NXPs AUTOSAR Real Time Drivers (RTDs) and other tools and framework (like SPD or SCST). NXP gives support to a number of compilers (NXP-GCC, IAR, DIAB and GHS) but we wish to use (Arm Compiler for Embedded FuSa) which is not in the last. 


1.                  Are there any ongoing efforts between NXP and ARM to add the ARM compiler to the list of compilers?  

2.                  Would NXP offer any technical support to help migrate from NXP GCC based compiler to the AMR Clang based compiler? For example re-run the unit tests for the RTDs or other tools using the new complier (with NXPs recommended options)? 


(https://developer.arm.com/Tools%20and%20Software/Arm%20Compiler%20for%20Embedded%20FuSa). 

Tags (2)
0 Kudos
Reply
1 Reply

1,571 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

1. Are there any ongoing efforts between NXP and ARM to add the ARM compiler to the list of compilers?

No. At least I am not aware of any as NXP added GCC support and GHS+IAR are supported from historic reasons.

2. Would NXP offer any technical support to help migrate from NXP GCC based compiler to the AMR Clang based compiler? For example re-run the unit tests for the RTDs or other tools using the new complier (with NXPs recommended options)?

Not sure here. Best is to rise a request at paid support:

https://www.nxp.com/support/support/nxp-engineering-services:SW-SUPPORT

Best regards,

Peter

0 Kudos
Reply