Freemaster example in S32 Design Studio for S32K144EVB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Freemaster example in S32 Design Studio for S32K144EVB

1,385件の閲覧回数
davorin_mista
Contributor I

S32 Design Studio includes two freemaster examples - is there any documentation on how to use/run them? I can build the example and load it to the target, but then I cannot figure out how to connect FreeMaster.

How do I run S32 and FreeMaster simultaneously? They seem to be competing for the same COM port.

 

 

0 件の賞賛
返信
1 返信

1,363件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Davorin,

It's not clear to me which freemaster example you are referring to.
I am testing the freemaster_s32k144 project in S32DS3.4+S32SDK RTM4.0.2. You can find the introduction document according to the description.txt.

freemaster_s32k144 description.png

freemaster_s32k144 doc.png

Following the example's documentation, I can run S32 and FreeMaster simultaneously.

freemaster_s32k144 pmp.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信