FreeMASTER3.1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,450件の閲覧回数
akhilranga
Contributor IV

 

 I am having trouble with connecting my #s32k144 to FreeMASTER 3.1. Every time i try to establish a connection the attached error pops up. i was using 115200. And i checked my COM port with openSDA enabled. I am not sure what else i need to do.  Can any one help me sort this thing out. Thanks in AdvanceScreenshot (116).png

0 件の賞賛
返信
1 解決策
2,445件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi akhilranga,

If you are follow the steps of Get Started with the S32K1xxEVB, then this may helps: Q&A of S32K1x FreeMASTER JumpStart Project

If you are create your own FreeMASTER project, please refer to: FreeMASTER How To

By the way, I am not able to access another question that you submitted: https://community.nxp.com/t5/S32K/s32k144-EVB-Flashing-Debugging-Error/td-p/1486806

Can you tell me if need help with that question?

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,446件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi akhilranga,

If you are follow the steps of Get Started with the S32K1xxEVB, then this may helps: Q&A of S32K1x FreeMASTER JumpStart Project

If you are create your own FreeMASTER project, please refer to: FreeMASTER How To

By the way, I am not able to access another question that you submitted: https://community.nxp.com/t5/S32K/s32k144-EVB-Flashing-Debugging-Error/td-p/1486806

Can you tell me if need help with that question?

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
2,440件の閲覧回数
akhilranga
Contributor IV

Hi Robin,

Thanks for the tips. Yes, i was following the steps of  Get Started with S32k1xxEVB .

And about the other question, https://community.nxp.com/t5/S32K/s32k144-EVB-Flashing-Debugging-Error/td-p/1486806. 

I have managed to resolve it.

 

0 件の賞賛
返信