FreeMASTER communication method question (S32K144W)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FreeMASTER communication method question (S32K144W)

ソリューションへジャンプ
4,372件の閲覧回数
SW_Park
Contributor II

Please check if FreeMASTER communication is possible with JTAG (Multilink) instead of UART.
1) Can I connect with the settings below?
  I haven't created a board yet, so I can't confirm it.
2) There is no JTAG setting macro in the software, what should I do?

Park_sang_woo_0-1640335480052.png

 

0 件の賞賛
返信
1 解決策
4,293件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

It is not necessary to change the separate macro option.

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
4,339件の閲覧回数
SW_Park
Contributor II

Thank you for answer.

I will use JTAG debug port instead of UART port, is SWD mode correct?

And how do I select options in the source?

0 件の賞賛
返信
4,311件の閲覧回数
SW_Park
Contributor II

So, is it not necessary to change the separate macro option?

Sangwoo_Park_0-1640580358418.png

 

0 件の賞賛
返信
4,294件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

It is not necessary to change the separate macro option.

0 件の賞賛
返信
4,322件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Sangwoo,

Please refer: 
Tools->Connection Wizard...

step1.pngstep2.pngstep3.pngstep4.pngstep5.pngstep6.pngXS32K14WEVB-Q064.jpg


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
4,348件の閲覧回数
ArchieLuo
Contributor III

If you are using PeMicro Multilink.

ArchieLuo_0-1640498231124.png

 

 

0 件の賞賛
返信