Framing error detection while TX in UART

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Framing error detection while TX in UART

1,176 Views
Sourdev
Contributor II

MCU - S9KEAZN64AMLC

We have a custom board used in LIN communication(UART based) with LIN transceiver while testing for LIN conformance we noticed one test case in which while TX from MCU the BIt error will be introduced, we need to detect it and generate an error response from MCU but while transmission from MCU, we are not able to see Bit error, in the datasheet it is mentioned that Error can be detected in RX  nothing mentioned regarding TX.

Is there any way to detect Framing or Noise errors while TX from MCU?

0 Kudos
Reply
0 Replies