Fls_Example_S32K148 : Can't debug program after flashing the example bianry for the first time.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Fls_Example_S32K148 : Can't debug program after flashing the example bianry for the first time.

Jump to solution
2,017 Views
Armang
Contributor II

Hello there, 

after flashing the binary of the example project Fls_Example_S32K148, it seems that some level of protection has been activated on the memory. And I can't debug my programs normally. 

Is this expected to happen when running the example?

0 Kudos
Reply
1 Solution
1,964 Views
Armang
Contributor II

I guess after flashing the example, the flash was locked. So I followed this post to perform production programming.

View solution in original post

0 Kudos
Reply
2 Replies
1,965 Views
Armang
Contributor II

I guess after flashing the example, the flash was locked. So I followed this post to perform production programming.

0 Kudos
Reply
1,982 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Armang 

Could you be more specific about what you mean by not being able to debug the project normally?

Besides that, could you tell me if you are using an EVB or if is it a custom board?

 

B.R.

VaneB

0 Kudos
Reply