Flexio Output trigger

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flexio Output trigger

Jump to solution
1,876 Views
584914019
Contributor III


The output trigger is equal to the timer output, and the signal form of the timer output depends on the working mode of the timer.
In order to ensure that the timer output can be sampled by the TRGMUX module, the width of the timer output high level and The working clock of the TRGMUX module is restricted. How to ensure it in actual application?

0 Kudos
Reply
1 Solution
1,865 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

The TRGMUX does not sample anything.

It is just connects one trigger source to one trigger input. 

danielmartynek_0-1604408118634.png

Best regards,

Daniel

View solution in original post

0 Kudos
Reply
1 Reply
1,866 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

The TRGMUX does not sample anything.

It is just connects one trigger source to one trigger input. 

danielmartynek_0-1604408118634.png

Best regards,

Daniel

0 Kudos
Reply