Flexio Output trigger

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flexio Output trigger

ソリューションへジャンプ
1,972件の閲覧回数
584914019
Contributor III


The output trigger is equal to the timer output, and the signal form of the timer output depends on the working mode of the timer.
In order to ensure that the timer output can be sampled by the TRGMUX module, the width of the timer output high level and The working clock of the TRGMUX module is restricted. How to ensure it in actual application?

0 件の賞賛
返信
1 解決策
1,961件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

The TRGMUX does not sample anything.

It is just connects one trigger source to one trigger input. 

danielmartynek_0-1604408118634.png

Best regards,

Daniel

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,962件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

The TRGMUX does not sample anything.

It is just connects one trigger source to one trigger input. 

danielmartynek_0-1604408118634.png

Best regards,

Daniel

0 件の賞賛
返信