FlexIO pin config

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FlexIO pin config

1,382 Views
yuegao1996
Contributor II

hi,

the manual says the pin can be

00b - Timer pin output disabled
01b - Timer pin open drain or bidirectional output enable
10b - Timer pin bidirectional output data
11b - Timer pin output

does this mean:

00- inpput and 11 - output

whats  ''01b'' and '10b' refer to ?

 

thanks!

0 Kudos
Reply
1 Reply

1,363 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

take a look at this description:

lukaszadrapa_0-1630671801678.png

Input, output and open drain are clear, I think. Bidirectional output then can be used to emulate data bus when you need both read and write operation on such bus.

Regards,

Lukas

0 Kudos
Reply