FlexCan is not initializing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FlexCan is not initializing

793件の閲覧回数
Rahul7384
Contributor I

We are using the S32K322 microcontroller with the NXP MCAL package driver for FlexCAN, specifically FlexCAN1. However, the driver is not initializing and we are encountering a timeout error. Another observation is that the driver performs a soft reset on FlexCAN but fails to set the property or encounters a timeout during this process. The MCU peripheral clock for FlexCAN is enabled, and we are using the example configuration for the S32K344."

 

 

タグ(1)
0 件の賞賛
返信
1 返信

737件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

be sure both a module and CAN PE clocks are enabled and active.  In asynchronous operation, the module clock frequency must always be greater than the PE clock freq.

BR, Petr

0 件の賞賛
返信