FlexCAN RX FIFO with Extended 29-Bit CAN IDs not Working

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

FlexCAN RX FIFO with Extended 29-Bit CAN IDs not Working

跳至解决方案
6,432 次查看
gbrowne
Contributor II

Hello.

I have run tests on the S32K144 with sending and receiving both standard (11-bit) and extended (29-bit) ID CAN frames.  What I have found is that I cannot receive extended ID frames when I use the RX FIFO, but I can receive standard ID frames.

Also, I can receive both standard and extended ID frames if I receive into a specific message buffer (i.e. the non-FIFO method).

So, is there something special to setting the RX FIFO to receive extended ID frames?  Is there working sample code for receiving extended ID frames with the RX FIFO?

Here is a general overview of my routines:

RX FIFO Routine (which only works for standard 11-bit ID frames):

FLEXCAN_DRV_Init(...)

FLEXCAN_DRV_SetRxMaskType(...)

FLEXCAN_DRV_SetRxFifoGlobalMask(...)

FLEXCAN_DRV_ConfigRxFifo(...)

FLEXCAN_DRV_ConfigTxMb(...)

FLEXCAN_DRV_Send(...)

FLEXCAN_DRV_RxFifoBlocking(...)

Specific Message Buffer Routine (which works for both standard 11-bit and extended 29-bit ID frames):

FLEXCAN_DRV_Init(...)

FLEXCAN_DRV_SetRxMaskType(...)

FLEXCAN_DRV_SetRxMbGlobalMask(...)

FLEXCAN_DRV_ConfigRxMb(...)

FLEXCAN_DRV_ConfigTxMb(...)

FLEXCAN_DRV_Send(...)

FLEXCAN_DRV_ReceiveBlocking(...)

Any insights would be much appreciated.

Thanks!

-Greg

1 解答
5,108 次查看
AnaAldescu
NXP Employee
NXP Employee

Hello Greg,

There is a known bug related to the Rx FIFO filters. If you're using other filter format than format A, extended ID's won't match the filter. This bug will be fixed in the next S32 SDK release.

If you're using format A for the ID filters, please make sure you configure the ID filter table with extended IDs:

flexcan_id_table_t filterTable[8U];

filterTable[0].id = 0x1FFFFFFF;
filterTable[0].isExtendedFrame = true;

FLEXCAN_DRV_ConfigRxFifo(INST_CANCOM1, FLEXCAN_RX_FIFO_ID_FORMAT_A, filterTable);

Please let me know if the problem is not solved.

Best regards,

Ana

在原帖中查看解决方案

2 回复数
5,109 次查看
AnaAldescu
NXP Employee
NXP Employee

Hello Greg,

There is a known bug related to the Rx FIFO filters. If you're using other filter format than format A, extended ID's won't match the filter. This bug will be fixed in the next S32 SDK release.

If you're using format A for the ID filters, please make sure you configure the ID filter table with extended IDs:

flexcan_id_table_t filterTable[8U];

filterTable[0].id = 0x1FFFFFFF;
filterTable[0].isExtendedFrame = true;

FLEXCAN_DRV_ConfigRxFifo(INST_CANCOM1, FLEXCAN_RX_FIFO_ID_FORMAT_A, filterTable);

Please let me know if the problem is not solved.

Best regards,

Ana

5,108 次查看
gbrowne
Contributor II

Ah, much appreciated Ana!

I was missing that extra isExtendedFrame flag in the filter table.

Thanks!

-Greg

0 项奖励
回复