FlexCAN_Ip_Example_S32K344 Rx interrupt problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FlexCAN_Ip_Example_S32K344 Rx interrupt problem

ソリューションへジャンプ
8,642件の閲覧回数
SudheerkumarA
Contributor II

Hi NXP Team,

I'm using the S32k3X4EVB board to test the "FlexCAN_Ip_Example_S32K344" example, and while I can send data over CAN correctly, reception is not occurring. "FlexCAN_Ip_Example_S32K344" project sample code is attached for your reference. If there are any CAN setup changes required in order to receive data over CAN with a Rx interrupt, do let me know

 

Regards,

Sudheer

0 件の賞賛
返信
1 解決策
8,630件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @SudheerkumarA,

This FlexCAN example configures the FlexCAN0 as a "Loopback". The Reference Manual describes loopback operation as:

"In this mode, FlexCAN performs an internal loopback that can be used for self-test operation. The bit stream output of the transmitter is fed back internally to the receiver input. The RX CAN input pin is ignored and the TX CAN output goes to the recessive state (logic 1). FlexCAN behaves as it normally does when transmitting and treats its own transmitted message as a message received from a remote node."

The received bits in the example are internally connected for testing purposes, this can be disabled by setting CTRL1[LPB] to 0b.

I hope you find this helpful!

Best regards,
Julián 

元の投稿で解決策を見る

0 件の賞賛
返信
7 返答(返信)
8,487件の閲覧回数
SudheerkumarA
Contributor II

Hi,

It's working.

 

Regards,

Sudheer

0 件の賞賛
返信
8,623件の閲覧回数
SudheerkumarA
Contributor II

Hi @Julián_AragónM ,

I've modified the FlexCAN operating mode setting to "normal or User mode" from "loopback" mode.

Please refer to the attachment for information on FlexCAN setups. Additionally, TAJ1043 was set up in Normal Mode by setting PTC20(STB) = High and PTC21(EN) = High on S32K3x4EVB-Q172 Hardware, however Rx interrupt is still not happening.

Please help me to solve this problem.

Regards,

Sudheer

タグ(2)
0 件の賞賛
返信
8,609件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @SudheerkumarA,

You can find a simple FlexCAN example over two boards in this community post:

Please help me testing this one instead, as the loopback example should be used for self-testing operations.

Best regards,
Julián.

0 件の賞賛
返信
8,590件の閲覧回数
SudheerkumarA
Contributor II

Hi @Julián_AragónM ,

I'll review the provided example. Is it possible to change the "FlexCAN_Ip_Example_S32K344" example to transmit and receive data via CAN in "user or normal" mode?

Please send it to us if there is a document available for configuring the FlexCAN with S32 DS so we can obtain additional details.

 

Regards,

Sudheer

0 件の賞賛
返信
8,588件の閲覧回数
SudheerkumarA
Contributor II

Hi @Julián_AragónM ,

The ".mex" file for the "Example_S32K344_FlexCAN_Ip_TX_RX_EnhanceRXFIFO_test_rtd200" example code is not opening for me. Is any another way I can examine this example?

We are using S32DS Vr 3.5 IDE; please see the attached for additional details regarding the problem.

Regards,

Sudheer

0 件の賞賛
返信
8,561件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @SudheerkumarA

This may be because of the version of the RTD or IDE, please help me confirming these are all set:

* Test HW: S32K3444EVB-Q172
* MCU: PS32K344EHVPBS 1P55A
* Compiler: S32DS.ARM.3.4
* SDK release: SW32K3_RTD_4_4_2_0_0_D2203
* Debugger: Lauterbach
* Target: internal_FLASH

Best regards,
Julián

0 件の賞賛
返信
8,631件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @SudheerkumarA,

This FlexCAN example configures the FlexCAN0 as a "Loopback". The Reference Manual describes loopback operation as:

"In this mode, FlexCAN performs an internal loopback that can be used for self-test operation. The bit stream output of the transmitter is fed back internally to the receiver input. The RX CAN input pin is ignored and the TX CAN output goes to the recessive state (logic 1). FlexCAN behaves as it normally does when transmitting and treats its own transmitted message as a message received from a remote node."

The received bits in the example are internally connected for testing purposes, this can be disabled by setting CTRL1[LPB] to 0b.

I hope you find this helpful!

Best regards,
Julián 

0 件の賞賛
返信