Flash tools:additional device problems

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash tools:additional device problems

1,736 Views
minjaekang99
Contributor I

Hello
We are using the s32k324 board.
An error occurred while debugging the board and laptop.
We need to build and debug the code.
Is there a way to fix this error? I'd appreciate it if you could tell me a new way instead of buying a debugger separately.

minjaekang99_1-1732541152978.pngminjaekang99_1-1732541152978.png

 

minjaekang99_0-1732541126880.pngminjaekang99_0-1732541126880.png

 



And while using the s32 flash tool, the target device does not have the s32k324 board set up. I read the user guide and it says to download the tool to use the additional device, what should I download?

minjaekang99_2-1732541166147.pngminjaekang99_2-1732541166147.png

 

 

0 Kudos
Reply
3 Replies

1,702 Views
minjaekang99
Contributor I

Thank you for your answer.
The file is now in version 344, but the same error occurs when I make the file again in version 324. Is it because the debugger version is low? I wonder if there is a solution.

0 Kudos
Reply

1,689 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @minjaekang99 

Sorry if I did not explain myself clearly.

A project created for a S32K344 will not work for a S32K324. You need to create a new application project with the corresponding MCU and then copy the application source files from your pre-existing project as well as any customizations you made to the project properties.

0 Kudos
Reply

1,715 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @minjaekang99 

Since the project was created for a S32K344 device, it will cause faults if used on a different device. The most viable option is to generate a new project with the corresponding MCU and then copy the application source files from your pre-existing project as well as any customizations you made to the project properties.

As for the S32 Flash Tool, it does not support S32K devices.

 

BR, VaneB

0 Kudos
Reply