Flash reliability S32K146

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flash reliability S32K146

ソリューションへジャンプ
3,571件の閲覧回数
eduard_reina
Contributor I

Hi Sr/ Mdm,

We are using S32K146 and as per datasheet requirements:

NVM reliability specifications when using as Program and Data Flash (attached picture):

nnvmcycp Cycling endurance 1 K — — cycles 2, 3

Does it mean that the maximum number of cycles per each Sector that NXP guarantee for this uC is 1K?

If we do more than 1K reflashing in a cycle test of code reflashing (same sectors), NXP doesn't guarantee the flash reliability after the 1K reflash? Even if reflash is done in a cycle test, thus, all of them during 1day?

Thank you in advance and best regards,

Eduard

タグ(1)
0 件の賞賛
返信
1 解決策
3,503件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Eduard,

This is the only specification available, min 1k cycles guaranteed across product temperature specification in Normal Mode (Table 25, footnote 2).

It is not the maximum number of cycles but the minimum number of cycles guaranteed.

Regards,

Daniel

元の投稿で解決策を見る

1 返信
3,504件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Eduard,

This is the only specification available, min 1k cycles guaranteed across product temperature specification in Normal Mode (Table 25, footnote 2).

It is not the maximum number of cycles but the minimum number of cycles guaranteed.

Regards,

Daniel