Fault Injection to cache locations using an interface provide in emcem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Fault Injection to cache locations using an interface provide in emcem

80件の閲覧回数
Rudved_3366
Contributor I

Hello @danielmartynek 

Good morning:-)

I have question regarding the fault injection to cache location:

I need to inject a 2-bit fault in Cache location but I'm not sure what it means as mentioned in the reference manual and we use NXP s32K394 microcontroller:

Rudved_3366_0-1791432690162.png

 

 

I need to call below function 2 times to inject the faults in cache and get the 2-bit error in cache like below: 

Rudved_3366_1-1791432699706.png

 

If I'm doing wrongly, could you please share the example code how to do this injection, and currently we are using SAF package in our project, so if there are already fault injection code exists for these, please share which file I need to refer to inject all kind of faults using (EIM) for memory test interface which is provided in SAF module.

0 件の賞賛
返信
1 返信

47件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信