FXLS90322 I2C Function

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FXLS90322 I2C Function

912 Views
Lin_SiuU
Contributor II

Hi :

I use S32K144 as MCU ,and the SDK Vision  is 4.0.2.

i Are there any Setting i must make before using the I2C communication Function of the FXLS90322?

I cannot receive the ACK bit from the slave while writing the address(the address had already moved over by 1 bit)

From the time sequence captured by oscilloscope, the time sequence of I2C is also normal, but still can not receive the ACK bit sent from the FXLS90322.

BTW,when I used FlexIO to simulate I2C communication, the error status I received was I2C_RX_Overrun

Looking forward for your reply.

@TomasVaverka 

0 Kudos
Reply
0 Replies