FX32K144HAT0MLLT/FS32K144HAT0MLLT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FX32K144HAT0MLLT/FS32K144HAT0MLLT

2,592 Views
JovialZ
Contributor I

Dear,

May I know FX32K144HAT0MLLT is the same as FS32K144HAT0MLLT? 

Thx!

0 Kudos
Reply
5 Replies

2,569 Views
JovialZ
Contributor I

Thx David!

However SDID value which is software functional related may be different.--Is it correct?

 

0 Kudos
Reply

2,565 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

There's no difference against between FX32K1 and FS32K1.

FXS32K... are just special ordering part numbers for incremental supply. Please contact local sales for help.

The System Device Identification Register (SDID) value in the FX part may be different than the SDID value of the FS part.

0 Kudos
Reply

2,292 Views
KLMan
NXP Employee
NXP Employee

Hi David,

In fact I was being ask by an NXP sales.

How SDID different between FS and FX considering they are of same on the other part of part number, e.g.FS32K146UAT0VLHT and FX32K146UAT0VLHT.

0 Kudos
Reply

2,571 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, is is the basically same device.

0 Kudos
Reply

2,331 Views
KLMan
NXP Employee
NXP Employee

same SDID? in case different is only FS and FS.

 

in RM, SDID is regarding memory size and feature set, etc, FS/FX was not mentioned.

0 Kudos
Reply