FTM PWM Output Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,996件の閲覧回数
chaitanya_kalyani
Contributor III

Hello,

I am facing issue for FTM PWM Output.

I observed issue is when I initialize the LPIT module.

But when I create a project with GCC then after initializing LPIT then also PWM is working as expected but when I create new project and choose IAR compiler instead of GCC then facing issue for PWM output in the same IAR project after commenting LPIT initialization then PWM is working as expected.

For my project LPIT is required. I am attaching both the sample project in the attachment (with GCC compiler and IAR compiler).

I am working on urgent project and quick response highly appreciated.

Thank you in advance.

0 件の賞賛
返信
1 解決策
2,982件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Your project seems to be a combination of lpit_periodic_interrupt_s32k142 and ftm_pwm_s32k142 code. I tried to combine these two project, did not find issue.

Please check the attached project. 

 

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,983件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Your project seems to be a combination of lpit_periodic_interrupt_s32k142 and ftm_pwm_s32k142 code. I tried to combine these two project, did not find issue.

Please check the attached project. 

 

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
2,967件の閲覧回数
chaitanya_kalyani
Contributor III

Hello @Robin_Shen ,

 

My problem is solved. Your test project helped me to solve my problem. 

0 件の賞賛
返信