FTM - Board compatibility / working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FTM - Board compatibility / working

4,571件の閲覧回数
nadreoh
Contributor II

Dear support Team,

 

Context:

I'm trying to use my FlexTimer module on DevBoard RevB (S32K144).

I also have the datasheet from Aug. 2015 and the new one from Aug. 2016.

I work with the IAR IDE, using the IAR library and a J-LINK Debugger.

 

My questions:

Is the FTM module able to work on my board (RevB)?

Or should I wait for the new board (from 2016)?

Or did I missed one or more configurations in my Code?

 

Note (from datasheet aug. 2015), page 801:

The Global Load mechanism of FTM module is not supported on this device.

 

My configurations:

It seems to approximately work when trying to Flash Code after several times and using:

• SOSC at 8MHz

• SPLL at 32MHz, that is also the System clock source (SYSclk/COREclk/BUSclk/SLOWclk set to 32MHz)

• SIRC / FIRC are disable

• FTM[0..3] clock source is SOSC_DIV1 (8MHz)

• PIN PTD15 / PTB5 set on Alteration2 to use FTM0_CH0 and FTM0_CH5 (same FTM0 Signal on this two PINs / channels)

• Need to generate a 4MHz PWM with Alpha, duty cycle = 50%

 

My Code (only for FTM):

 Following the datasheet 2016 advice (page 1086) for my configuration. Uncalled Registers are set as Default.

 

int main (void)

{

   Disable WatchDog

   Oscillators initialization

   Ports initialization

 

  /* Needs to set MOD to get only one incrementation */

  FTM0_MOD |= FTM_MOD_MOD(0x0001u);

 

  /* Needs to set Channels MODES to edge-aligned PWM */
  FTM0_C0SC |= FTM_C0SC_MSB(1u);
  FTM0_C0SC |= FTM_C0SC_ELSA(1u);
  FTM0_C5SC |= FTM_C5SC_MSB(1u);
  FTM0_C5SC |= FTM_C5SC_ELSA(1u);
 

  /* Needs to set CnV to get flag when Counter value is 1 */
  FTM0_C0V |= FTM_C0V_VAL(0x0001u);
  FTM0_C5V |= FTM_C5V_VAL(0x0001u);
 

  /* Others configurations... */
  FTM0_CNT |= FTM_CNT_COUNT(0x0000u);
  FTM0_SC |= FTM_SC_CLKS(3u);
  FTM0_SYNC |= FTM_SYNC_SYNCHOM(1u);
  FTM0_SYNCONF |= FTM_SYNCONF_SWOM(1u);
  FTM0_SYNCONF |= FTM_SYNCONF_SWRSTCNT(1u);
  FTM0_SYNCONF |= FTM_SYNCONF_SYNCMODE(1u) ;
 

  /* Enable FTM0_CH0 and FTM0_cH5 */
  FTM0_OUTMASK |= FTM_OUTMASK_CH7OM(1u);
  FTM0_OUTMASK |= FTM_OUTMASK_CH6OM(1u);
  FTM0_OUTMASK |= FTM_OUTMASK_CH5OM(0u);
  FTM0_OUTMASK |= FTM_OUTMASK_CH4OM(1u);
  FTM0_OUTMASK |= FTM_OUTMASK_CH3OM(1u);
  FTM0_OUTMASK |= FTM_OUTMASK_CH2OM(1u);
  FTM0_OUTMASK |= FTM_OUTMASK_CH1OM(1u);
  FTM0_OUTMASK |= FTM_OUTMASK_CH0OM(0u);
 

  /* Active matching channels */
  FTM0_SYNC |= FTM_SYNC_SWSYNC(1u);
  FTM0_SC |= FTM_SC_PWMEN0(1u);
  FTM0_SC |= FTM_SC_PWMEN5(1u);

 

Main Loop

 

Best regards,

Nadreoh

ラベル(1)
5 返答(返信)

4,177件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

Yes, the Global Load mechanism of FTM module is not supported on cut1 device (mask 0N77P).

The global load mechanism allows several FTM modules to have their double buffered registers synchronously reloaded after a synchronization event. In your code just FTM0 is used, so this feature is not needed.

The FTM should work. Or you do not see PWM waveform on the outputs?

BR, Petr

0 件の賞賛
返信

4,177件の閲覧回数
nadreoh
Contributor II

Thank a lot for your answer.

I have tried some others configurations to understand how to generate PWM thanks to the FlexTimers, but it's not clear to me.

 

 

What I Need

I need an 8MHz PWM Signal coming from the FlexTimer0 with a 50% duty cycle.

 

 

What I've done

  • SOSC = 8MHz

  • SPLL = 20 (MULT) * 8 SOSC / (2 (SPLL FACTOR) * 2 (DIV1) * (4 + 1 (PREDIV))  )

      → [16 MHz for SPLL] & [8 MHz for SPLLDIV1]

NOTE : it seems that the "+ 1" applied to the PreDivider is ignored on my board (Rev B). Is that a problem? I have to set PreDivider to 5 instead of 4 (+ 1).

 

  • System clock is given by the SPLL clock : CORE = BUS = SLOW = SYS = 16MHz

 

  • Using only FTM0 (same Code as above) on channel 0 (for the red LED) and channel 5 to output the signal on PIN PTB5.

 

  • I refered to the illustration given in the attachment to configure FTM0 as PWM with a 50% duty cycle :

FTM_MOD_MOD(0x0001u);

FTM_C5V_VAL(0x0001u);

FTM_SC_PS(0u);

FTM0_CNTIN = 0x0000ul;

 PWM_on_FTM.PNG

 

What I have

 

With the DIV1 set to "2", I got a PWM signal of 4MHz (8MHz from SPLLDIV1 is divided by 2 because the FTM needs one clock cycle to set up and one more to set down).

I tried to set the DIV1 to "1", but this time I didn't get any signal on FTM0. Why can't I set DIV1 to "1"? Are there any limits applied on FTM, system clock, PORTB or whatever?

Best regards,

Nadreoh

0 件の賞賛
返信

4,177件の閲覧回数
nadreoh
Contributor II

* The "+1" applied on PreDivider is coming from the configuration, this Problem is resolved. Remains the SPLLDIV1 Parameter problem...

0 件の賞賛
返信

4,177件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi Nadreoh,

If external clock is selected as the FTM counter clock, then its freq must not exceed ¼ of the FTM system clock.

Try to select FTM system clock as a counter clock, using FTM0_SC |= FTM_SC_CLKS(1u), and update PWM modulo according FTM system clock.

BR, Petr

4,177件の閲覧回数
nadreoh
Contributor II

That was my missing Information :

If external clock is selected as the FTM counter clock, then its freq must not exceed ¼ of the FTM system clock.

Thank you for Reply, it works the way I want,

Nadreoh

0 件の賞賛
返信