FS32K142UAT0VLFT I2C supports clock stretching or not

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FS32K142UAT0VLFT I2C supports clock stretching or not

ソリューションへジャンプ
1,355件の閲覧回数
ultra12
Contributor III

Dear Team,

I am using FS32K142UAT0VLFT in my design .

I would like to know whether this controller supports I2C clock stretching or not

Regards

HARI

0 件の賞賛
返信
1 解決策
1,338件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信
3 返答(返信)
1,343件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello Hari,

Yes, it does.

LPI2C in Master mode supports clock stretching by default.

In Slave mode, it is configurable (Slave Configuration Register 1).

 

Regards,

Daniel

0 件の賞賛
返信
1,342件の閲覧回数
ultra12
Contributor III

Hi Daniel,

Thank you very much for the info.

May I know in general How to check if a microcontroller I2C supports clock stretching or not.

Can I say , if the minimum frequency is 0Hz (and/or there's no maximum time for the low period of the clock), that indicates it is clock stretching compatible.

Regards

HARI

0 件の賞賛
返信
1,339件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Do you mean in Master mode?

If so, refer to this thread:

https://community.nxp.com/t5/S32K/How-does-S32K148-LPI2C-master-support-clock-stretching-feature/m-p...

 

Regards,

Daniel

 

0 件の賞賛
返信