FS32K MPU using MCUXpresso IDE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FS32K MPU using MCUXpresso IDE

3,144件の閲覧回数
huang_hw
Contributor II
I am trying to develop using FS32K MPU (FS32K148UJT0VLQT). The development tool that is recommended on NXP web-site is "S32 Design Studio IDE for Arm® based MCUs".

Since this is a new project, I thought the IDE "MCUXpresso IDE" should be used as this is the new IDE that NXP will support and develop.

Question: For a new project using FS32K148, should the "MUXpresso IDE" or "S32 Design Studio IDE for Arm based MCUs' be used?

Thanks.

タグ(2)
0 件の賞賛
返信
1 返信

2,582件の閲覧回数
razva_tilimpea
NXP Employee
NXP Employee

Hi,

For S32K1xx devices please use S32 Design Studio IDE for Arm. This is the tool designed for S32K1xx devices, so it provides an better integrations with gdb, debuggers etc. Also, SDK is compatible just with Design Studio.

Probably with extra effort you can start your project in MCUXpresso IDE, but it is targeted for Kinetis devices.

Best regards,

Razvan