FS26 device Real-Time Drivers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FS26 device Real-Time Drivers

Jump to solution
3,169 Views
pagdav
Contributor III

Dear all,

I found an error in the FS26 Device Real-Time Drivers and in particular in the following version:

S32K3XX FS26 AUTOSAR R21-11 Version 2.0.1

In the function SchM_Exit_Sbc_fs26_SBC_FS26_EXCLUSIVE_AREA_00(), defined in the file .\RTD\src\SchM_Sbc_fs26.c, the variable reentry_guard_SBC_FS26_EXCLUSIVE_AREA_01 shall be replaced with reentry_guard_SBC_FS26_EXCLUSIVE_AREA_00 and the variable msr_SBC_FS26_EXCLUSIVE_AREA_01 with msr_SBC_FS26_EXCLUSIVE_AREA_00.

Thank you for your support.

0 Kudos
Reply
1 Solution
2,977 Views
CongDang
NXP Employee
NXP Employee

yes, it was ready resolved in S32K3xx_SBC_FS26_R21-11_3.0.0.

View solution in original post

0 Kudos
Reply
3 Replies
3,082 Views
CongDang
NXP Employee
NXP Employee

Thanks for your reporting!

I raised a bug ticket for it.

0 Kudos
Reply
2,984 Views
pagdav
Contributor III

Dear @CongDang,

could you confirm that the bug has been resolved in the version S32K3XX FS26 AUTOSAR R21-11 Version 3.0.0?

Best regards,

@davpag 

0 Kudos
Reply
2,978 Views
CongDang
NXP Employee
NXP Employee

yes, it was ready resolved in S32K3xx_SBC_FS26_R21-11_3.0.0.

0 Kudos
Reply