Hello Community,
I am working with the FRDM-A-S32K344 (S32K344MINI-EVB) board using:
- S32DS 3.5.8
- RTD 4.0.0 (R21-11)
I successfully imported and built the I2c_Ip_Example_S32K344_Q172 project and reviewed the existing configuration.
After reviewing the board user manual, I noticed that the default LPI2C bus is connected to several onboard I²C devices, including the FXLS8964 accelerometer, P3T1750 temperature sensor.
I would like to evaluate LPI2C in Master mode and communicate with one of the onboard slave devices (preferably the FXLS8964 or P3T1750).
Could you please provide:
- Recommended configuration for LPI2C Master mode.
- Any available example project for FRDM-A-S32K344.
- Guidance on reading data from the onboard sensors using the I2c_Ip driver.
Any example project, application note, or reference implementation would be greatly appreciated.
Thank you for your support.
Best Regards,
Veer