FLEXIO SPI without SDK example?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FLEXIO SPI without SDK example?

Jump to solution
3,052 Views
janSiroky
Contributor II

Hi everybody!

 

I am wondering if there is some SPI example project using FLEXIO without SDK?

 

All i have found is

1. flexio spi sdk example project

2. flexio uart example project

 

Thanks

Jan

0 Kudos
Reply
1 Solution
3,047 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Jan,

There is a non-sdk SPI FLEXIO example in

AN12174 Using FlexIO to emulate communications and timing peripherals

https://www.nxp.com/docs/en/application-note/AN12174.pdf

AN12174SW

https://www.nxp.com/webapp/Download?colCode=AN12174SW&docLang=en

 

Regards,

Daniel

View solution in original post

3 Replies
3,048 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Jan,

There is a non-sdk SPI FLEXIO example in

AN12174 Using FlexIO to emulate communications and timing peripherals

https://www.nxp.com/docs/en/application-note/AN12174.pdf

AN12174SW

https://www.nxp.com/webapp/Download?colCode=AN12174SW&docLang=en

 

Regards,

Daniel

3,037 Views
janSiroky
Contributor II

Thanks a lot!

Have a nice day.

Jan

0 Kudos
Reply
2,686 Views
ywjack
Contributor III

Hi :

These flexio DEMOs without SDK use polling, can you give a DEMO for interrupt processing? Regarding flexio's simulation of UART using interrupt mode, without SDK

0 Kudos
Reply