FLEXCAN module on RTD for S32K311

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

FLEXCAN module on RTD for S32K311

跳至解决方案
3,471 次查看
simonjuanr
Contributor II

Hello all,

I'm migrating a project from S32K312 to S32K311. It seems like everything is similar, but when I try to configure the CAN interface with FLEXCAN, I cannot find this module in the pin configuration tool. Also mention that in the peripheral view, it does appear.

I checked the S32KXXX datasheet and this microcontroller contains 3 FLEXCAN channels.

My question is: Does anyone know if it is not implemented yet, but it will be in the future?

 

SDK: PlatformSDK_S32K3_S32K311_M7

Version: 3.0.0

Device: S32K311

 

Thanks in advance.

标记 (4)
0 项奖励
回复
1 解答
3,394 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @simonjuanr 

The SW team just abbreviated the name in ConfigTools. So, it is the same. 

在原帖中查看解决方案

0 项奖励
回复
3 回复数
3,440 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @simonjuanr 

Could you share an image of the driver you can add with the peripherals tool?

Also, are you using low-level drivers (IP) or high-level drivers (MCAL)?

 

B.R.

VaneB

0 项奖励
回复
3,427 次查看
simonjuanr
Contributor II

Hi @VaneB ,

I can select FLEXCAN driver from low-level drivers, as you can see:

simonjuanr_0-1698912079830.png

 

The problem is, when configuring the proper pins, I cannot attach those pins to FLEXCAN module, as I did for S32K312.

S32K312 pin view:

simonjuanr_2-1698912279484.png

 

S32K311 pin view:

simonjuanr_1-1698912243552.png

As you can see, modules in 311 are called "CAN", not "FLEXCAN" as before. I don't know if it's just a typo, but I want to be sure what I'm doing.

 

Thanks in advance,

Simón

0 项奖励
回复
3,395 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @simonjuanr 

The SW team just abbreviated the name in ConfigTools. So, it is the same. 

0 项奖励
回复