FLASH_DRV_ProgramSection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FLASH_DRV_ProgramSection

2,100 Views
814420552
Contributor III

hello,

when i set FlexSAM to traditional SRAM and erase all flash memory, SRAM boot and when call the following code, why the address 0x6000 is always 0xFFFFFFFF?

whether is it wrong way to use the function FLASH_DRV_ProgramSection?

I expected 1024 data can be write to flash memory by call function FLASH_DRV_ProgramSection.

for(i= 0; i< 1024; i++)
{
*(uint8_t *)(0x14000000 + i) = sourceBuffer[i % 255];

}
ret = FLASH_DRV_ProgramSection(&flashSSDConfig, 0x6000, 1024);

wish your help

0 Kudos
Reply
1 Reply

2,053 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello Kui Wu,


If you look at the description of this command it explains the previous steps you need to do before calling this command:

 

pastedImage_2.png

 

Also, remember that the sector size is 2KB.

Best Regards,
Alexis Andalon

0 Kudos
Reply